Part Number: TMS320F2808
Other Parts Discussed in Thread: C2000WARE
Hi,
I am working on a 2808 based project which is built on ccs3.3. Compile on ccs, debug and release have no
problem at all. Now we import this project into ccs 11. Ccs 11 can compile the project and download the
out file to the DSP. But after downloading the DSP is not working. I use ccs 11 load the out file to the
DSP to generated in ccs3.3 and it works fine.
I made a lot of effort and did the same compilation settings on CCS 11 as the original settings, but it
just didn't work, and the breakpoint was said out of memory when debugging.
I also tried to import the project into various versions of CCS, including CCS 4, CCS 6.2, CCS 7 and CCS
10.1.1, all of which can generate out files, but after the out files are downloaded to the DSP, the DSP
does not Work. Could it be that CCS is not compatible with the 2808 device?
Thank you very much.