Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE
Hi all,
I was checking the sci bootloader example for f28002x . (flash_kernelex3_sci_flash_kernel). in this project , " FlashAPI_F28002x_FPU32.lib" is used for flash operation. Can i use " FlashAPI_ROM_F28002x_FPU32.lib" instead to reduce the code size ? if possible, what are the changes i have to made on the project ?
thanks
-Sudheesh