Part Number: TIDM-1000
We implemented the Vienna code in our own hardware design and it works well but the controller loses control of the output voltage below 300W.
Design specs:
Fsw = 140 kHz
Design load = 8 kW
DC output = 400 VDC
AC input = 208 VAC
There is no mention of minimum load in the user guide.
We noticed that vienna_Gv_out goes negative right at the minimum load point.
We tried to implement a bang-bang wrapper wherein we shut off PWM when DC output exceeds 415 V and re-enable at 385 V but it appears to latch off when Vout exceeds 415.
We initially scaled the voltage and current through the GUI and as far as I know, offsets are not automatically zeroed out (this is another task - figure out how and when auto calibration of voltage and current sensing happens).
Question 1) What is the cause of regulation loss below 300 W?
Also, when we implemented build mode 4, the DC balance controller did not perform well - it was unstable. When I lowered the switching frequency down to about 80 kHz in steps, it got progressively better.
Question 2) What is the likely cause? Not enough time to perform the balance algorithm? Is the CLA required at this switching frequency?
So far we are able to keep the buses balanced with only a few watts worth of load resistors, so the balance loop may not be necessary.