Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28379D
Hi,
Does TI provide a pin list in excel for the TMS320F28379D?
Thanks!
Regards,
Michael
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28379D
Hi,
Does TI provide a pin list in excel for the TMS320F28379D?
Thanks!
Regards,
Michael
I was asking for the part but if you have it for the controlcard I would take that too. This is my first time using the Delfino and I am custom to getting a pin list for the device where I can define the signals and etc to pass back and forth between me and the FW engineer. Is there something like that?
Michael
Michael,
The pinout of controlCARD is available in C2000Ware release.
C:/ti/c2000/C2000Ware_4_01_00_00/boards/controlCARDs/TMDSCNCD28379D/R1_3/TMDSCNCD28377D_180cCARD_pinout_R1_3.pdf
I have exported the file in excel format and is attached here.
TMDSCNCD28377D_180cCARD_pinout_R1_3.xlsx
Thanks & Regards,
Santosh
This is for the control card but I am looking for the actual part pin list in excel. I would have thought there would be a pin list for the BGA and the other packages in excel. I have already had to recreate it for the BGA but I hope to migrate to the 177 pin package part and thus will have to do it again.
Michael,
Yes, unfortunately we do not have part pin-list in excel format which we can share.
Thanks & Regards,
Santosh