This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025C: Sample project code for the control of a BLDC using hall sensors

Part Number: TMS320F280025C
Other Parts Discussed in Thread: CONTROLSUITE, C2000WARE

TMS320F280025C: Do you have a sample project code for the control of a BLDC using hall sensors?

We are using DRV8323RS board.

When I try to enable MOTOR1_HALL define, with MOTOR1_ISBLDC with universal_motorcontrol_lab_f28002x project, I am getting the following error during building.

"ISBLDC can't work with other estimaor simultaneously"

Is there another project that allows me to use BLDC with hall?

Please advice.