Part Number: TMS320F28377S
Hello expert,
I am asking this question for our customer.
The customer uses TMS320f28377S, the CCS version and the compiler version are shown in the figure below.

Customer find that when the uninitialized data is allocated, if the addresses assigned by .ebss, .esystem, .cio and .data contain addresses after 0x10000, the program cannot run, and the following figure will be displayed after debugging.

For example, in the following figure, .ebss, .esystem, .cio, and .data are allocated to addresses before 0x10000, which can be debugged normally.
For example, if .ebss, .esystem, .cio, and .data in the figure below are allocated to addresses after 0x10000, the problem mentioned above will occur.
Since I don't have the EVM of the F28277S, I used the F28379D for testing, and I can't reproduce the customer's problem. I noticed that CIO is displayed in the upper left corner of the console table. Is it a problem of .cio allocation? Could you please kindly help me analyze it? I'm attaching the customer's .cmd file below
// The user must define CLA_C in the project linker settings if using the
// CLA C compiler
// Project Properties -> C2000 Linker -> Advanced Options -> Command File
// Preprocessing -> --define
#define CLA_C
#ifdef CLA_C
// Define a size for the CLA scratchpad area that will be used
// by the CLA compiler for local symbols and temps
// Also force references to the special symbols that mark the
// scratchpad are.
CLA_SCRATCHPAD_SIZE = 0x200;
--undef_sym=__cla_scratchpad_end
--undef_sym=__cla_scratchpad_start
#endif //CLA_C
MEMORY
{
PAGE 0 :
/* BEGIN is used for the "boot to SARAM" bootloader mode */
D01SARAM : origin = 0x00BF00, length = 0x000100
RAMM0 : origin = 0x000122, length = 0x0002DE
Cla1Prog : origin = 0x008000, length = 0x002000
RAMGS0_6 : origin = 0x00C000, length = 0x007000
RESET : origin = 0x3FFFC0, length = 0x000002
/* Flash sectors */
BEGIN : origin = 0x084002, length = 0x000004
FLASH_HEAD : origin = 0x084000, length = 0x000002
FLASH_HEAD2 : origin = 0x084006, length = 0x000002
FLASHC_N : origin = 0x084008, length = 0x037FF8 /* on-chip Flash */
FLASH_SAFETY_CRC : origin = 0x0BC000, length = 0x000001
FLASH_SAFETY : origin = 0x0BC001, length = 0x003FFD
FLASH_TRAIL : origin = 0x0BFFFE, length = 0x000002
PAGE 1 :
BOOT_RSVD : origin = 0x000002, length = 0x000120 /* Part of M0, BOOT rom will use this for stack */
RAMM1 : origin = 0x000400, length = 0x000400
RAMD01 : origin = 0x00B000, length = 0x000F00
Cla1Share : origin = 0x00A000, length = 0x000A00 /* for CLA Data RAM */
Cla1Stack : origin = 0x00AA00, length = 0x000500 /* for CLA Stack Ram*/
RAMSafetyCla : origin = 0x00AF00, length = 0x000100 /* for CLA Stack Ram*/
RAMGS7_14 : origin = 0x013000, length = 0x008000 /* for Ram Data */
CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080
CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080
RAMSafetyPrt : origin = 0x01B000, length = 0x000900
RAM_SAFETY_dwregister0 : origin = 0x01B900, length = 0x000002
RAM_SAFETY_dwregister1 : origin = 0x01B902, length = 0x000002
RAM_SAFETY_dwregister2 : origin = 0x01B904, length = 0x000002
RAM_SAFETY_wregister0 : origin = 0x01B906, length = 0x000001
RAM_SAFETY_wregister1 : origin = 0x01B907, length = 0x000001
RAM_SAFETY_wregistercheckFlag : origin = 0x01B908, length = 0x000001
RAMSafety : origin = 0x01B909, length = 0x0006F7
}
SECTIONS
{
/* Allocate program areas: */
.cinit : > FLASHC_N PAGE = 0, ALIGN(4)
.binit : > FLASHC_N PAGE = 0, ALIGN(4)
.pinit : > FLASHC_N, PAGE = 0, ALIGN(4)
.text : > FLASHC_N PAGE = 0, ALIGN(4)
codestart : > BEGIN PAGE = 0, ALIGN(4)
/* Initalized sections go in Flash */
.const : > FLASHC_N PAGE = 0, ALIGN(4)
.econst : > FLASHC_N PAGE = 0, ALIGN(4)
.switch : > FLASHC_N PAGE = 0, ALIGN(4)
.args : > FLASHC_N PAGE = 0, ALIGN(4)
/* Allocate uninitalized data sections: */
.stack : > RAMM1 PAGE = 1
.ebss : > RAMGS7_14 PAGE = 1
.esysmem : > RAMGS7_14 PAGE = 1
.cio : > RAMGS7_14 PAGE = 1
.data : > RAMGS7_14 PAGE = 1
#ifdef __TI_COMPILER_VERSION__
#if __TI_COMPILER_VERSION__ >= 15009000
.TI.ramfunc : {} LOAD = FLASHC_N,
RUN = RAMGS0_6,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#else
ramfuncs : LOAD = FLASHC_N,
RUN = RAMGS0_6,
LOAD_START(_RamfuncsLoadStart),
LOAD_SIZE(_RamfuncsLoadSize),
LOAD_END(_RamfuncsLoadEnd),
RUN_START(_RamfuncsRunStart),
RUN_SIZE(_RamfuncsRunSize),
RUN_END(_RamfuncsRunEnd),
PAGE = 0, ALIGN(4)
#endif
#endif
ProgramRamFuncs : LOAD = FLASHC_N, /* Used by InitFlash() in SysCtrl.c */
RUN = RAMGS0_6,
LOAD_START(_ProgramRamFuncs_loadstart),
LOAD_END(_ProgramRamFuncs_loadend),
RUN_START(_ProgramRamFuncs_runstart)
PAGE = 0, ALIGN(4)
FPUmathTables : > FLASHC_N PAGE = 0
FlashSafetyCRC : > FLASH_SAFETY_CRC PAGE = 0
FlashSafety : > FLASH_SAFETY PAGE = 0
FlashHead : > FLASH_HEAD PAGE = 0
FlashHead2 : > FLASH_HEAD2 PAGE = 0
FlashTrail : > FLASH_TRAIL PAGE = 0
Cla1Prog : LOAD = FLASHC_N,
RUN = Cla1Prog,
RUN_START(_Cla1ProgRunStart),
LOAD_START(_Cla1ProgLoadStart),
LOAD_SIZE(_Cla1ProgLoadSize),
PAGE = 0, ALIGN(4)
CLAData : > Cla1Share, PAGE = 1
RAMSafetyForCla : > RAMSafetyCla, PAGE = 1
Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1
CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1
RAMSafetyForPrt : > RAMSafetyPrt, PAGE = 1
RamSafety_dwregister0 : > RAM_SAFETY_dwregister0 PAGE = 1
RamSafety_dwregister1 : > RAM_SAFETY_dwregister1 PAGE = 1
RamSafety_dwregister2 : > RAM_SAFETY_dwregister2 PAGE = 1
RamSafety_wregister0 : > RAM_SAFETY_wregister0 PAGE = 1
RamSafety_wregister1 : > RAM_SAFETY_wregister1 PAGE = 1
RamSafety_wregistercheckFlag : > RAM_SAFETY_wregistercheckFlag PAGE = 1
// Must be allocated to memory the CLA has write access to
CLAscratch :
{ *.obj(CLAscratch)
. += CLA_SCRATCHPAD_SIZE;
*.obj(CLAscratch_end) } > Cla1Stack, PAGE = 1
.scratchpad : > Cla1Stack, PAGE = 1
.bss_cla : > Cla1Stack, PAGE = 1
.reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
Best Regards,
Julia