Part Number: TMS320F28388D
Hello,
I'm writing some applicaiton which acts as an bootloader and flash writer for firmware update.
But I'm struck in some problem. It has ended up that it fails to jump to the secondary application from the bootloader app.
The code of my own boot application for jumping to the second app is like below.
//
// Included Files
//
#include "driverlib_cm.h"
#include "cm.h"
#define APP_START_ADDRESS 0x00270000U
void exit(uint32_t address){
//
// Jump to entry address
//
__asm(" bx r0");
}
//
// Main
//
void main(void)
{
CM_init();
GPIO_writePin(120U,0);
exit(APP_START_ADDRESS);
}
//
// End of File
//
and the link command script is the same as below.
MEMORY
{
/* Flash sectors */
CMBANK0_RESETISR : origin = 0x00200000, length = 0x00000008 /* Boot to Flash Entry Point */
CMBANK0_SECTOR0 : origin = 0x00200008, length = 0x00003FF8
CMBANK0_SECTOR1 : origin = 0x00204000, length = 0x00004000
CMBANK0_SECTOR2 : origin = 0x00208000, length = 0x00004000
C1RAM : origin = 0x1FFFC000, length = 0x00002000
C0RAM : origin = 0x1FFFE000, length = 0x00002000
BOOT_RSVD : origin = 0x20000000, length = 0x00000800 /* Part of S0, BOOT rom will use this for stack */
S0RAM : origin = 0x20000800, length = 0x00003800
S1RAM : origin = 0x20004000, length = 0x00004000
S2RAM : origin = 0x20008000, length = 0x00004000
S3RAM : origin = 0x2000C000, length = 0x00004000
E0RAM : origin = 0x20010000, length = 0x00004000
CPU1TOCMMSGRAM0 : origin = 0x20080000, length = 0x00000800
CPU1TOCMMSGRAM1 : origin = 0x20080800, length = 0x00000800
CMTOCPU1MSGRAM0 : origin = 0x20082000, length = 0x00000800
CMTOCPU1MSGRAM1 : origin = 0x20082800, length = 0x00000800
CPU2TOCMMSGRAM0 : origin = 0x20084000, length = 0x00000800
CPU2TOCMMSGRAM1 : origin = 0x20084800, length = 0x00000800
CMTOCPU2MSGRAM0 : origin = 0x20086000, length = 0x00000800
CMTOCPU2MSGRAM1 : origin = 0x20086800, length = 0x00000800
}
SECTIONS
{
.resetisr : > CMBANK0_RESETISR
.vftable : > CMBANK0_SECTOR0 /* Application placed vector table in Flash*/
.vtable : > S0RAM /* Application placed vector table in RAM*/
.text : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.cinit : > CMBANK0_SECTOR0
.pinit : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.switch : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.sysmem : > S2RAM
.stack : > C1RAM
.ebss : > C1RAM
.econst : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
.esysmem : > C1RAM
.data : > S3RAM
.bss : > S3RAM
.const : >> CMBANK0_SECTOR0 | CMBANK0_SECTOR1
MSGRAM_CM_TO_CPU1 : > CMTOCPU1MSGRAM0, type=NOINIT
MSGRAM_CM_TO_CPU2 : > CMTOCPU2MSGRAM0, type=NOINIT
MSGRAM_CPU1_TO_CM : > CPU1TOCMMSGRAM0, type=NOINIT
MSGRAM_CPU2_TO_CM : > CPU2TOCMMSGRAM0, type=NOINIT
.TI.ramfunc : {} LOAD = CMBANK0_SECTOR0,
RUN = C0RAM,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
The link command of the secondary application where the bootapp above is trying to jump to is like this,
MEMORY
{
/* Flash sectors */
CMBANK0_RESETISR10 : origin = 0x00270000, length = 0x00000008 /* Boot to Flash Entry Point */
CMBANK0_SECTOR10_11 : origin = 0x00270008, length = 0x00007FF8
CMBANK0_SECTOR12 : origin = 0x00278000, length = 0x00004000
CMBANK0_SECTOR13 : origin = 0x0027C000, length = 0x00004000
C1RAM : origin = 0x1FFFC000, length = 0x00001FFF
C0RAM : origin = 0x1FFFE000, length = 0x00001FFF
BOOT_RSVD : origin = 0x20000000, length = 0x00000800 /* Part of S0, BOOT rom will use this for stack */
S0RAM : origin = 0x20000800, length = 0x000037FF
S3RAM : origin = 0x2000C000, length = 0x00003FFF
S1_S3RAM : origin = 0x20004000, length = 0x0000BFFF
E0RAM : origin = 0x20010000, length = 0x00003FFF
CPU1TOCMMSGRAM0 : origin = 0x20080000, length = 0x00000400
CPU1TOCMMSGRAM0_ECAT : origin = 0x20080400, length = 0x00000400
CPU1TOCMMSGRAM1 : origin = 0x20080800, length = 0x00000800
CMTOCPU1MSGRAM0 : origin = 0x20082000, length = 0x00000400
CMTOCPU1MSGRAM0_ECAT : origin = 0x20082400, length = 0x00000400
CMTOCPU1MSGRAM1 : origin = 0x20082800, length = 0x00000800
CPU2TOCMMSGRAM0 : origin = 0x20084000, length = 0x00000800
CPU2TOCMMSGRAM1 : origin = 0x20084800, length = 0x00000800
CMTOCPU2MSGRAM0 : origin = 0x20086000, length = 0x00000800
CMTOCPU2MSGRAM1 : origin = 0x20086800, length = 0x00000800
}
SECTIONS
{
.resetisr : > CMBANK0_RESETISR10, ALIGN(8)
.vftable : > CMBANK0_SECTOR10_11, ALIGN(8) /* Application placed vector table in Flash*/
.vtable : > S0RAM /* Application placed vector table in RAM*/
.text : >> CMBANK0_SECTOR10_11 | CMBANK0_SECTOR12, ALIGN(8)
.cinit : > CMBANK0_SECTOR10_11, ALIGN(8)
.pinit : > CMBANK0_SECTOR10_11, ALIGN(8)
.switch : > CMBANK0_SECTOR10_11, ALIGN(8)
.sysmem : > C1RAM
.stack : > C1RAM
.ebss : > C1RAM
.econst : > CMBANK0_SECTOR10_11, ALIGN(8)
.esysmem : > C1RAM
.data : >> C0RAM|C1RAM
.bss : > C0RAM
.const : > CMBANK0_SECTOR10_11, ALIGN(8)
MSGRAM_CM_TO_CPU1 : > CMTOCPU1MSGRAM1, type=NOINIT
MSGRAM_CM_TO_CPU1_ECAT : > CMTOCPU1MSGRAM0_ECAT, type=NOINIT
MSGRAM_CM_TO_CPU2 : > CMTOCPU2MSGRAM0, type=NOINIT
MSGRAM_CPU1_TO_CM : > CPU1TOCMMSGRAM0, type=NOINIT
MSGRAM_CPU1_TO_CM_ECAT : > CPU1TOCMMSGRAM0_ECAT, type=NOINIT
MSGRAM_CPU2_TO_CM : > CPU2TOCMMSGRAM0, type=NOINIT
.TI.ramfunc : {} LOAD = CMBANK0_SECTOR10_11,
RUN = S1_S3RAM,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
I'm not sure why it doesn't works well although the locations of application are different.
I would really appreciate it if you could tell me how to do that correctrly.