Part Number: TMS320F280025
Other Parts Discussed in Thread: AMC1302
Hello,
customer wants to use isolated amplifier AMC1302 to measure currents. It outputs differential signals. How to input these signals into the F280025?
Regards, Holger
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F280025
Other Parts Discussed in Thread: AMC1302
Hello,
customer wants to use isolated amplifier AMC1302 to measure currents. It outputs differential signals. How to input these signals into the F280025?
Regards, Holger
You may find the reference design or EVM on the web pages for AMC1302, and select the right shunt resistor according to the measurement signals, and then connect the output of the AMC1302 to the ADC pins of the F280025C.
https://www.ti.com/product/AMC1302
Hello Yanming,
the AMC1302 has differentieal outputs. How to connect to the F280025 ADC? Can we connect differential signals to the F280025 ADC?
Regards, Holger

Please refer to the application below.
Interfacing a Differential-Output (Isolated) Amp to a Single-Ended Input ADC (Rev. A)
Hi Yanming,
I don't know how this link will solve my questions. Please give me an detailed answer otherwise I have to ask the app guys from C2000 PL directly!
Regards, Holger
Add an amplifier to convert the differential output to single-ended output (0~3.3V) for the ADC input of the F280025C as the circuit in the application note.
Interfacing a Differential-Output (Isolated) Amp to a Single-Ended Input ADC (Rev. A)

Hi Yanming,
thanks for the answer. Is it also possible to use 2 ADC F280025 inputs instead of the OpAmp?
Regards, Holger
Hi Holger,
thanks for the answer. Is it also possible to use 2 ADC F280025 inputs instead of the OpAmp?
What you are referring to is pseudo differential. Theoretically it should work but there are some practical limitations which you will ran into. For this to work well, the 2 ADCs have to be matched exactly for all specifications like offset, gain, linearity etc but in reality they are not. This will in turn introduce more errors into your system because the 2 ADCs are not perfectly matched. You will be better of using a differential to single-ended opamp as Yanming suggested.