Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hello,
I am configuring the system clock to 100MHz and the low speed clock to 25MHz. I tried to place in a NOP statement with a GPIO toggle and noticed that the pin toggled WAY slower than I expected (1.6mS). So then I tried to measure the XCLKOUT to verify my clock frequency. I selected INTOSC2 as the XCLKOUT source and can see that it is running with a period of 400nS or 1.25MHz which makes no sense to me? The reference manual states it should be running at 10MHz. I also tried to measure INTOSC1 and also saw the same frequency as the measured INTOSC2. Below is a screen shot of my logic analyzer and register configurations.
I am running off a custom board right now since the LAUNCHPAD dev kit does not breakout the XCLKOUT GPIO. But looking at my NOP test case on the LAUNCHPAD dev kit, I see the same 1.6mS timing so I am assuming this issue is consistent between boards.


Thanks