Other Parts Discussed in Thread: CCSTUDIO
Hi,
I am trying to use IQmath.h library for fixed point trigonometric functions, like sine cosine & tangent inverse,
my Q format is _Q13
After including IQmath.h, when i compile the code, its sucessfull but when i build it following error occurs:
Linking...] "C:\CCStudio_v3.3\C6000\cgtools\bin\cl6x" -@"Debug.lkf"
<Linking>
>> error: bad long filename table for '|ø|'
>> Compilation failure
Build Complete,
2 Errors, 0 Warnings, 0 Remarks
kindly help me besides, same problem has occurred to some of my other friends...
part of the code is:
void ofdm_sig(short m1[],int s_real[],int s_imag[])
{
short i;
for(i=0;i<P2;i++)
{
s_real[i]=_IQ13cos(m1[i]);
s_imag[i]=_IQ13sin(m1[i]);
}
}
void angle_msg(int s_real[],int s_imag[],short angle[])
{
short i;
for(i=0;i<P2;i++)
{
angle[i]=(short)(_IQ13atan2(s_imag[i],s_real[i]));
}
}