Part Number: TMDSCNCD280039C
Other Parts Discussed in Thread: C2000WARE
I am able to download using external XDS110 Debug probe but when I thy do download using USB-C I get error -260.

As specified in the error message I used xdsdfu to download the latest firmware as well as tried to set the serial number. The serial number did not seem to work.

I noticed that when I connect the external debug probe I can see that it uses COM3 and COM4 in the device manager whereas when I connect the USB-C the device is unknown. That make is seem like a windows driver is missing but I do not know where to get it.
The external device is disconnected from the PC's USB and from the developer board when the download fails.
2 S1 switches are both on. I have tried different positions.
Your help would be most appreciated.