This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: EMIF issue

Part Number: TMS320F28377D


Hi team,

Here's an issue from the customer may need your help:

The customer would like to know why is EM1WE pulled low twice during a write. The test EMIF module waveforms are shown below:

Could you help check this case? Thanks.

Best Regards,

Cherry

  • Cherry,

        Could you provide some more information? What mode of the EMIF is being used? What is the EMIF connected to? Is it possible to share the schematics privately?

  • Hi Hareesh,

    Thanks for your help.

    The code is as follows:

    //###########################################################################
    //
    // FILE: emif1_16bit_asram.c
    //
    // TITLE: EMIF1 module accessing 16bit ASRAM.
    //
    //! \addtogroup cpu01_example_list
    //! <h1> EMIF ASYNC module (emif1_16bit_asram)</h1>
    //!
    //! This example configures EMIF1 in 16bit ASYNC mode
    //! This example uses CS2 as chip enable.
    //!
    //! \b Watch \b Variables: \n
    //! - \b TEST_STATUS - Equivalent to \b TEST_PASS if test finished correctly,
    //! else the value is set to \b TEST_FAIL
    //! - \b ErrCount - Error counter
    //!
    //
    //###########################################################################
    //
    // $Release Date: $
    // $Copyright:
    // Copyright (C) 2013-2022 Texas Instruments Incorporated - http://www.ti.com/
    //
    // Redistribution and use in source and binary forms, with or without
    // modification, are permitted provided that the following conditions
    // are met:
    //
    // Redistributions of source code must retain the above copyright
    // notice, this list of conditions and the following disclaimer.
    //
    // Redistributions in binary form must reproduce the above copyright
    // notice, this list of conditions and the following disclaimer in the
    // documentation and/or other materials provided with the
    // distribution.
    //
    // Neither the name of Texas Instruments Incorporated nor the names of
    // its contributors may be used to endorse or promote products derived
    // from this software without specific prior written permission.
    //
    // THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
    // "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
    // LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
    // A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
    // OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
    // SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
    // LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
    // DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
    // THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
    // (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
    // OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
    // $
    //###########################################################################
    
    //
    // Included Files
    //
    #include "F28x_Project.h"
    
    
    #define ASRAM_CS2_START_ADDR 0x100000
    #define ASRAM_CS2_SIZE 0x8000
    
    
    //
    // Globals
    //
    Uint16 ErrCount = 0;
    Uint32 TEST_STATUS;
    int i;
    
    //
    // Function Prototypes
    //
    extern void setup_emif1_pinmux_async_16bit(Uint16);
    
    
    // mem_read_write - This function performs simple read/write word accesses to memory.
    char mem_read_write(Uint32 start_addr, Uint32 mem_size)
    {
    //unsigned long mem_rds;
    unsigned long mem_wds;
    long *XMEM_ps;
    //unsigned int i;
    
    //Write data
    XMEM_ps = (long *)start_addr;
    
    //Fill memory
    mem_wds = 0x1;
    //for (i=0; i < mem_size; i++)
    //{
    //*XMEM_ps++ = mem_wds;
    *XMEM_ps = mem_wds;
    // mem_wds += 0x11111111;
    //}
    
    /*
    //Verify memory
    mem_wds = 0x01234567;
    XMEM_ps = (long *)start_addr;
    for (i=0; i < mem_size; i++)
    {
    mem_rds = *XMEM_ps;
    if( mem_rds != mem_wds)
    {
    return(1);
    }
    XMEM_ps++;
    mem_wds += 0x11111111;
    }
    */
    return(0);
    }
    
    void main(void)
    {
    char ErrCount_local;
    //TEST_STATUS = TEST_FAIL;
    
    //
    // Initialize system control
    //
    InitSysCtrl();
    
    DINT;
    
    //
    // Initialize the PIE control registers to their default state.
    // The default state is all PIE interrupts disabled and flags
    // are cleared.
    // This function is found in the F2837xD_PieCtrl.c file.
    //
    InitPieCtrl();
    //
    // Disable CPU interrupts and clear all CPU interrupt flags:
    //
    EALLOW;
    IER = 0x0000;
    IFR = 0x0000;
    EDIS;
    
    //
    // Initialize the PIE vector table with pointers to the shell Interrupt
    // GService Routines (ISR).
    // This will populate the entire table, even if the interrupt
    // is not used in this example. This is useful for debug purposes.
    // The shell ISR routines are found in F2837xD_DefaultIsr.c.
    // This function is found in F2837xD_PieVect.c.
    //
    InitPieVectTable();
    
    //
    //Configure to run EMIF1 on full Rate (EMIF1CLK = CPU1SYSCLK)
    //
    EALLOW;
    ClkCfgRegs.PERCLKDIVSEL.bit.EMIF1CLKDIV = 0x0;
    EDIS;
    
    EALLOW;
    //
    // Grab EMIF1 For CPU1
    //
    Emif1ConfigRegs.EMIF1MSEL.all = 0x93A5CE71;
    if(Emif1ConfigRegs.EMIF1MSEL.all != 0x1)
    {
    ErrCount++;
    }
    
    //
    //Disable Access Protection (CPU_FETCH/CPU_WR/DMA_WR)
    //
    Emif1ConfigRegs.EMIF1ACCPROT0.all = 0x0;
    if(Emif1ConfigRegs.EMIF1ACCPROT0.all != 0x0)
    {
    ErrCount++;
    }
    
    //
    // Commit the configuration related to protection. Till this bit remains set
    // content of EMIF1ACCPROT0 register can't be changed.
    //
    Emif1ConfigRegs.EMIF1COMMIT.all = 0x1;
    if(Emif1ConfigRegs.EMIF1COMMIT.all != 0x1)
    {
    ErrCount++;
    }
    
    //
    // Lock the configuration so that EMIF1COMMIT register can't be
    // changed any more.
    //
    Emif1ConfigRegs.EMIF1LOCK.all = 0x1;
    if(Emif1ConfigRegs.EMIF1LOCK.all != 1)
    {
    ErrCount++;
    }
    
    EDIS;
    EALLOW;
    GpioCtrlRegs.GPBDIR.bit.GPIO32 = 1;//Configuration direction: 0 input; 1 output 
    GpioCtrlRegs.GPBDIR.bit.GPIO33 = 1;
    GpioCtrlRegs.GPBPUD.bit.GPIO32 = 0;//Pullup: 0 enables pullup; 1 disables pullup 
    GpioCtrlRegs.GPBPUD.bit.GPIO33 = 0;
    GpioDataRegs.GPBCLEAR.bit.GPIO32 = 1;//Data clear: Writing a 0 has no effect; writing a 1 pulls low 
    GpioDataRegs.GPBCLEAR.bit.GPIO33 = 1;//Data clear: Writing a 0 has no effect; writing a 1 pulls low 
    
    EDIS;
    //
    //Configure GPIO pins for EMIF1
    //
    setup_emif1_pinmux_async_16bit(0);
    
    
    Emif1Regs.ASYNC_CS2_CR.bit.ASIZE = 1;//1:0
    Emif1Regs.ASYNC_CS2_CR.bit.TA= 10; //3:2
    //Emif1Regs.ASYNC_CS2_CR.bit.R_HOLD= 0;//6:4
    //Emif1Regs.ASYNC_CS2_CR.bit.R_STROBE = 0;//12:7
    //Emif1Regs.ASYNC_CS2_CR.bit.R_SETUP = 0;//16:13
    Emif1Regs.ASYNC_CS2_CR.bit.W_HOLD =0;//19:17
    Emif1Regs.ASYNC_CS2_CR.bit.W_STROBE =2;//25:20
    Emif1Regs.ASYNC_CS2_CR.bit.W_SETUP =0;//29:26
    Emif1Regs.ASYNC_CS2_CR.bit.EW = 0;//30
    Emif1Regs.ASYNC_CS2_CR.bit.SS = 0;//31
    while (1)
    {
    ErrCount_local = mem_read_write(ASRAM_CS2_START_ADDR, ASRAM_CS2_SIZE);
    ErrCount = ErrCount + ErrCount_local;
    DELAY_US(100);
    }
    }

    What mode of the EMIF is being used?

    Asynchronous mode.

    What is the EMIF connected to?

    The development board is used and writes are performed inside the main function.

    The EM1CS3,EM1WE,EM1D0 of the development board is measured directly at the schematic J5 port.

    Is it possible to share the schematics privately?

    https://e2echina.ti.com/cfs-file/__key/communityserver-discussions-components-files/56/28377_955E7F679F530674FE56_.pdf

    https://e2echina.ti.com/cfs-file/__key/communityserver-discussions-components-files/56/28377_3868C35F7F67_.pdf

    https://e2echina.ti.com/cfs-file/__key/communityserver-discussions-components-files/56/CCS9.2_5F00_28377D_5F00_CPU1.rar

    Thanks and regards,

    Cherry

  • Cherry,

        This appears to be the same issue discussed in this post