Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSCNCD28388D, TMDSHSECDOCK, TMDSFSIADAPEVM
Hi
Thanks and Best regards,
Tsurumoto.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28388D
Other Parts Discussed in Thread: TMDSCNCD28388D, TMDSHSECDOCK, TMDSFSIADAPEVM
Hi
Thanks and Best regards,
Tsurumoto.
Tsurumoto-San,
The TMDSCNCD28388D +TMDSHSECDOCK +TMDSFSIADAPEVM EVMs can be powered by the included USB cables. There is no need for an external power supply. If you want to use an external AC adapter you need a 5V power supply >1A. The connector should be a Center positive Barrel Plug, 2.5mm I.D. x 5.5mm O.D. x 10.0mm. The 10mm number can be a little longer or shorter, this is the length of the plug.
I don't know how long this link will work, but I filtered by Voltage and connector, be sure to verify the amperage/wattage.
Please note that when using TMDSFSIADAPEVM with TMDSCNCD28388D you will need to jump 3.3V power from the TMDSHSECDOCK to TMDSFSIADAPEVM because it uses the older FSI standard connector. This is covered in the User's Guide.
https://www.ti.com/lit/pdf/swru555
Regards,
Cody
Cody - Thanks for the reply. I have purchased a power supply with a 5.5 x 2.5 mm barrel connector, and have confirmed that it does fit.