Part Number: TMS320F280041
Hello,
I am writing an application requiring low power mode. In the image below from the TMS320F28004x Datasheet, it is advertised that when using DC-DC in Halt mode I should "typically" see 1.7 + 0.2 ~ 1.9mA on the 3V3 line feeding Vddio and Vdda. I am, however, seeing more like 14mA. I am disabling flash and PLL, but I am still seeing these results. Could you please advise?

Listed below is my low power mode function running from RAM.
#pragma CODE_SECTION(lpm_enterLowPowerMode, "ramfuncs");
void lpm_enterLowPowerMode(void)
{
/* Unlock locked registers */
EALLOW;
/* Check the arguments. */
ASSERT(Flash_isCtrlBaseValid(FLASH0CTRL_BASE));
/* Write the power mode to the appropriate register. */
HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) = (HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) & ~((FLASH_FBFALLBACK_BNKPWR0_M) << ((uint32_t) FLASH_BANK0 * 2U))) | ((uint32_t) FLASH_BANK_PWR_SLEEP << ((uint32_t) FLASH_BANK0 * 2U));
/* Write the power mode to the appropriate register. */
HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) = (HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) & ~((FLASH_FBFALLBACK_BNKPWR0_M) << ((uint32_t) FLASH_BANK1 * 2U))) | ((uint32_t) FLASH_BANK_PWR_SLEEP << ((uint32_t) FLASH_BANK1 * 2U));
/* Write the power mode to the appropriate register. */
HWREG(FLASH0CTRL_BASE + FLASH_O_FPAC1) = (HWREG(FLASH0CTRL_BASE + FLASH_O_FPAC1) & ~(uint32_t) FLASH_FPAC1_PMPPWR) | (uint32_t) FLASH_PUMP_PWR_SLEEP;
/* Set Idle to Halt */
HWREG(CPUSYS_BASE + SYSCTL_O_LPMCR) = (HWREG(CPUSYS_BASE + SYSCTL_O_LPMCR) & ~(uint32_t) SYSCTL_LPMCR_LPM_M) | SYSCTL_LPM_HALT;
/* Disable PLL */
HWREGH(CLKCFG_BASE + SYSCTL_O_SYSPLLCTL1) &= ~(SYSCTL_SYSPLLCTL1_PLLCLKEN | SYSCTL_SYSPLLCTL1_PLLEN);
/* Enter Halt Mode */
IDLE;
/* Power Up Flash */
/* Write the power mode to the appropriate register. */
HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) = (HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) & ~((FLASH_FBFALLBACK_BNKPWR0_M) << ((uint32_t) FLASH_BANK0 * 2U))) | ((uint32_t) FLASH_BANK_PWR_ACTIVE << ((uint32_t) FLASH_BANK0 * 2U));
/* Write the power mode to the appropriate register. */
HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) = (HWREG(FLASH0CTRL_BASE + FLASH_O_FBFALLBACK) & ~((FLASH_FBFALLBACK_BNKPWR0_M) << ((uint32_t) FLASH_BANK1 * 2U))) | ((uint32_t) FLASH_BANK_PWR_ACTIVE << ((uint32_t) FLASH_BANK1 * 2U));
/* Write the power mode to the appropriate register. */
HWREG(FLASH0CTRL_BASE + FLASH_O_FPAC1) = (HWREG(FLASH0CTRL_BASE + FLASH_O_FPAC1) & ~(uint32_t) FLASH_FPAC1_PMPPWR) | (uint32_t) FLASH_PUMP_PWR_ACTIVE;
EDIS;
}