This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I have implemented a DFU over CAN, where the bootloader checks, if the application header is correct (a key) or not. To start a DFU, the application should modify the header to 0x0000, such that
the bootloader notice, that the firmware needs to be updated. I implemented a small program to test, if I can overwrite some flash data by using the Fapi_issueProgrammingCommand(), but the overwrite process always fails with a 0x48 error:
/////////////////////////////////////////////////////////////////////////////////////////////////////Reset Flash header //Init flash first: initFlashSectors(); EALLOW; uint16_t miniBuffer1[4] = {0x0000}; uint16_t miniBuffer2[4] = {0x0000}; miniBuffer1[0] = 0x46ab; miniBuffer1[1] = 0x17c4; miniBuffer1[2] = 0x1289; miniBuffer1[3] = 0x3ffe; //////////////////////////////////////////////////////////////////////////////////////////////////////Write first to flash header Fapi_issueProgrammingCommand((uint32_t *) 0x0008F000, miniBuffer1, sizeof(miniBuffer1), 0, 0, Fapi_AutoEccGeneration); while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}; Fapi_FlashStatusType oFlashStatus = Fapi_getFsmStatus(); //////////////////////////////////////////////////////////////////////////////////////////////////////Write to zero now Fapi_issueProgrammingCommand((uint32_t *) 0x0008F000, miniBuffer2, sizeof(miniBuffer2), 0, 0, Fapi_AutoEccGeneration); while (Fapi_checkFsmForReady() != Fapi_Status_FsmReady){}; oFlashStatus = Fapi_getFsmStatus(); EDIS; /////////////////////////////////////////////////////////////////////////////////////////////////////Reset Flash header if(oFlashStatus) //Error occured { while(1) { // // Delay // GPIO_togglePin(34); DEVICE_DELAY_US(1e5); // GPIO_togglePin(31); } } else { while(1) //No error occured { // // Delay // GPIO_togglePin(31); DEVICE_DELAY_US(1e6); // GPIO_togglePin(31); } }
How can the data at a specific flash area be modified (of course with 0x0000, otherwise it will not work), without erasing the sector?