Part Number: TMS320F28377D
Other Parts Discussed in Thread: TMS320F28379D, LMV844, THS4531
We are using a F28377DPTPEP chip on our own PCB, and we are experiencing an issue with the ADC measurements.
The issue is that the ADC measurements have random noise in some samples when measuring signals around 1.5V.
To diagnose the problem:
- We are measuring a constant signal of 1.5V.
- We are using only SOC0 in the ADCD.
- We are triggering measurements at constant intervals of around 300us.
- We are triggering the measurements only by sw.
- We are using a DAC to output the measured signal and compare the input and the output in real time with an oscilloscope.
- The voltage in the input pin is perfectly constant as measured by the oscilloscope.
- The DAC is not the problem since we tested a constant value and it works with perfect accuracy.
We have tested several sample and hold scale factors. In all of them the noise is similar.
We have also tested several resistances and capacitors in the input pin: With very small values the input signal is distorted, but with higher and mid values (currently 680Ohm, 100nF) the input signal is not distorted but the measurements are still noisy. Our circuit on the input is as follows: Voltage follower -> resistance -> input pin 56 (PTP format, ADCIND0) + capacitor to ground.
We believe this is not a hardware issue since we tested also on a LAUNCHPAD XL TMS320F28379D v2.0 and we are getting similar results.
Below I include an image taken with the oscilloscope where C2 is the signal in the ADC input pin and C1 is the signal in the DAC output pin.