This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: The PowerPAD layout

Part Number: TMS320F28377S

Hi champs,

My customer is using 176-PIN F28377S and wants to know more about the PowerPAD layout, please advise your comments on below questions,

  1. In datasheet we suggest 0.2 mm diameter via and Application Report slma002h suggests 0.33 mm diameter via, which suggestion is better?
  2. On the back of PowerPAD, what method is recommended to get better heat dissipation? Is there any risk if customer uses bare copper like the front of PowerPAD?

Regards,

Luke

  • Hi Luke,

    In datasheet we suggest 0.2 mm diameter via and Application Report slma002h suggests 0.33 mm diameter via, which suggestion is better?

    Either would be fine, see info from App Note below. The 0.33mm via should offer higher current capacity and be able to transfer more heat.

    On the back of PowerPAD, what method is recommended to get better heat dissipation? Is there any risk if customer uses bare copper like the front of PowerPAD?

    Do you mean for the backside of the PCB (i.e. side the C2000 is not soldered onto)? I don't see any specific guidance on this in the datasheet or App Note. I suppose you could put some external heat-sink on the backside if deemed necessary.

    Best,

    Kevin

  • Kevin,

    Yes, I meant for the backside of the PCB. As you mentioned, we don't have any specific guidance on this.

    Do you see any concern if customer uses bare copper on the backside of PowerPAD area?

    Regards,

    Luke

  • Hi Luke,

    It's OK to do and a heatsink could be soldered onto the back even. Only concern is something could touch and short to the exposed copper on the back side of the board, but this may not be a concern in some designs.

    Best,

    Kevin