This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: TMS320F28379D

Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE

Dear all,

I have two TMS320F28379D launchpad controllers. I am creating my code through matlab 2019b. The first controller works properly. On the other hand, I cannot programm the second 28379D launchpad.

Although I can connect to it and also upload my programm through CCS, when i try to enable Real-time mode and run the controller i get the following error message:

"C28xx_CPU1: Trouble Reading Register PC: (Error -1142 @ 0x0) Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation. (Emulation package 9.3.0.00042) ".

Has anyone came across this problem before? Thank you in advance.