Part Number: TIDM-1000
Dear team:
Customers have the following problems with this reference design:
1. The inductance value calculated on page 13 of the user's guide does not match through simulation. Current simulation ripple measured by reference design is about half of the ripple marked in guide. Does the actual current ripple of TI match? Is there a reference waveform?
2. It is necessary to add an AC N-point to the midpoint of the capacitor when opening the loop test according to the reference design. Is there any line without N-line test? Customer simulation tests are voltage stable, but capacitor voltage is extremely unbalanced.
3. For the first step open-loop test, after the customer considers adding DC voltage, first measure single-phase BOOST and then two-phase BOOST. Is this feasible?
Best regards,
Green