Other Parts Discussed in Thread: C2000WARE
Dear team:
My customer referred to the IPC Lab, CPU2 routine of 28377 in the C2000 academy, and made the following interrupt settings:
void main(void) { // Configure system clock and PLL, enable peripherals, and configure // flash if used. Device_init(); // Initialize the PIE module and vector table. // Interrupt_initModule(); // Interrupt_initVectorTable(); Interrupt_initModule(); Interrupt_initVectorTable(); // Clear any IPC flags if set already IPC_clearFlagLtoR(IPC_CPU2_L_CPU1_R, IPC_FLAG_ALL); // Enable IPC0 interrupt. IPC_registerInterrupt(IPC_CPU2_L_CPU1_R, IPC_INT0, ipc0_ISR); // Enable global interrupts. EINT; // Enable real-time debug. ERTM; // Synchronize both the cores. IPC_sync(IPC_CPU2_L_CPU1_R, IPC_FLAG17); for (;;) { // Do nothing. NOP; } } interrupt void ipc0_ISR(void) { uint32_t cmd, addr, data; // num = 4824; // Clear interrupt flags. Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP1); // Read the data from the IPC registers. num = IPC_readCommand(IPC_CPU2_L_CPU1_R, IPC_FLAG0, false, &cmd, &addr, &data); // Acknowledge IPC1 flag from remote. IPC_ackFlagRtoL(IPC_CPU2_L_CPU1_R, IPC_FLAG0); // J[0] = cmd; J[1] = addr; J[3] = data; }
After setting as above, the register can be set using IPC_sendcommand, but the IPC0 interrupt of CPU2 cannot be started.
Also attach the cmd file:
SECTIONS { /* Allocate program areas: */ .cinit : > FLASHE PAGE = 0, ALIGN(4) .init_array : > FLASHE, PAGE = 0, ALIGN(4) .text : >> FLASHB|FLASHC|FLASHD|FLASHE PAGE = 0, ALIGN(4) codestart : > BEGIN PAGE = 0, ALIGN(4) /* Allocate uninitalized data sections: */ .stack : > RAMM1 PAGE = 1 .data : > RAMGS15 PAGE = 1 .bss : >> RAMGS3 PAGE = 1 .sysmem : > RAMGS2 PAGE = 1 /* Initalized sections go in Flash */ .const : >> FLASHF | FLASHG | FLASHH PAGE = 0, ALIGN(4) .switch : > FLASHB PAGE = 0, ALIGN(4) .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ GROUP { .TI.ramfunc { -l sfra_f32_tmu_eabi.lib } ramfuncs } LOAD = FLASHD, RUN = RAMGS0GS1, LOAD_START(RamfuncsLoadStart), LOAD_SIZE(RamfuncsLoadSize), LOAD_END(RamfuncsLoadEnd), RUN_START(RamfuncsRunStart), RUN_SIZE(RamfuncsRunSize), RUN_END(RamfuncsRunEnd), PAGE = 0, ALIGN(4) /* The following section definitions are required when using the IPC API Drivers */ GROUP : > CPU1TOCPU2RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > CPU2TOCPU1RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } SFRA_F32_Data : > RAMGS2, ALIGN = 64, PAGE = 1 SFRA_Data : > RAMGS2, ALIGN = 64, PAGE=1 FPUmathTables : > FLASHN, PAGE = 0 .scratchpad : > RAMLS0LS1, PAGE = 1 .bss_cla : > RAMLS0LS1, PAGE = 1 controlVariables : > RAMLS0LS1, PAGE = 1 .const_cla : LOAD = FLASHH, RUN = RAMLS2LS3LS4LS5, RUN_START(Cla1ConstRunStart), LOAD_START(Cla1ConstLoadStart), LOAD_SIZE(Cla1ConstLoadSize), PAGE = 0 GROUP { isrcodefuncs dclfuncs } LOAD = FLASHH, RUN = RAMLS2LS3LS4LS5, LOAD_START(isrcodefuncsLoadStart), LOAD_SIZE(isrcodefuncsLoadSize), LOAD_END(isrcodefuncsLoadEnd), RUN_START(isrcodefuncsRunStart), RUN_SIZE(isrcodefuncsRunSize), RUN_END(isrcodefuncsRunEnd), PAGE = 0, ALIGN(4) /* CLA specific sections */ Cla1Prog : LOAD = FLASHH, RUN = RAMLS2LS3LS4LS5, LOAD_START(Cla1ProgLoadStart), RUN_START(Cla1ProgRunStart), LOAD_SIZE(Cla1ProgLoadSize), PAGE = 0, ALIGN(4) Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 MSGRAM_CPU1_TO_CPU2 : > CPU1TOCPU2RAM, PAGE = 1 MSGRAM_CPU2_TO_CPU1 : > CPU2TOCPU1RAM, PAGE = 1 }
Best regards,
Green