Part Number: TMS320F28069M
Other Parts Discussed in Thread: TMS320F28379D,
Hello,
Is it possible to configure the ADC as differential (rather than single-ended) on all C2000 microcontrollers? Specifically I'm wondering about whether that's possible for the TMS320F28069M microcontroller because I don't see any mention of that on the datasheet for the TMS320F28069M. For the TMS320F28379D microcontroller that I've used in the past, it says on the datasheet that the ADCs can be configured as either 12 bit single-ended signals or 16-bit differential signals. However since it doesn't say anything anything similar on the TMS320F28069M datasheet, does that mean that differential ADCs are not possible on the TMS320F28069M microcontroller?
Thanks,
Kevin