This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377S: EMIF1 connect external SRAM data abnormal

Part Number: TMS320F28377S
Other Parts Discussed in Thread: C2000WARE

Dear expert,

My customer uses emif1 CS2 to connect an external RAM, memory address starting at 0x100000
He writes data for 0x100000, for example, 0×1234, However, the address 0x100001 will automatically change to 0x1234. Similarly, he writes data 0x5678 to address 0x100001, and the data in address 0x100000 will automatically change to 0x 5678. Both addresses are bound
The addresses that follow are the same problem. The data is the same for every two addresses.