Other Parts Discussed in Thread: TMS320F28379D
Hello, I am trying to use usb_flash_programmer with F28379D, using Launch Pad XL TMS320F28379D.
I have connected Launch Pad to PC, set boot selector switch to 1 and set CTS to 0. Then I reset hardware and turn on usb_flash_programmer. programmer.exe, enter the command "usb_flash_programmer.exe F2837xD_usb_flash_kernels_cpu01.dat blinky_cpu01.dat",

according to the assumption that the computer should recognize the device and indicate that the installation of the driver failed, by our own installation of the driver. But my device manager did not recognize the USB device and did not prompt to install the driver, only the three device drivers associated with the XDS100V2.



What is my operation that may cause this problem?
Best regards, thanks!