Part Number: TMS320F280049C
Other Parts Discussed in Thread: TMS320F28379D,
The C2000 Position Manager BISS-C Library User's Guide shows TMS320F28379D configured for BiSS on figure 3 page 6. (Shown below)
1) can this be implemented using TMS320F280049C?
2) GPIO7 shows the SPI being clocked by the CLB via and external pin connection. Can this be done using the XBARs without the external connection?
3) Is there an example CCS project for BiSS using the TMS320F280049C ?
We are currently in hardware selection stage for this project.
Thanks for your help
Shiraz