Part Number: TMS320F280049C
Other Parts Discussed in Thread: TMDXIDDK379D, C2000WARE
Hi,
I just need confirmation on the limitations of sensorless FOC control.
We are currently testing our prototype PMSM inverter (based on an Infineon driver) controlled by the TMS320F280049C Launchpad and the sensorless FOC example solutions from C2000 Motor Control SDK 4.00. An external PID controller closes the servo loop and controls the motor via a PWM signal to the Launchpad for torque control.
Everything seems to work well even at quite low speed, however for servo control I think we will need to add a sensor (A/B/Z encoder -> QEP) for low/zero speed control.
Can you confirm that this is correct, and is it feasible for the InstaSPIN-MOTION sensored software to work with an external PID controller, i.e. for it to only use the encoder information for commutation and let the external controller handle the position/speed.
Any advice/examples would be greatly appreciated.