Other Parts Discussed in Thread: TMS320F2810
i'm using the tms320f2810 chip(clock frequency : 150MHz). in the datasheet it is given that maximum IO(GPIO) buffer speed is limited to 20MHz.
1. why it is limited to 20MHz?
2. What will happen if i toggle the GPIO pin more that 20MHz?
3. What is is maximum rate at which i can toggle IO pin safely?
Reference :
Data Manual
Literature Number: SPRS174J
April 2001 - Revised December 2003
page : 108
thanks
Arun Gopalakrishnan