This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: motor automatically shut down

Part Number: TMS320F28027

dear 

         TMS320F28027FPTT under the power supply of 3.3 v, using the hvlab05b library, without any software protection, the motor automatically shut down, and the state machine will still be in normal operation? After shutdown, found that the speed of less than 100 RPM, maintain 6 seconds, the host began to alarm, the current volume of 300, there are 5 problems

 

Is there any advise ?thanks in advance