Part Number: TMS320F280025C
Hi Champs,
Here is my case:
HW: F280025C LP
Step 1: Flash the MCU by using CCS + XDS110. I am NOT using debug mode.
Step 2: remove the XDS110 without removing the power supply. The MCU runs normally.
Step 3: Under receiving a command via UART, the MCU resets itself by using the API SysCtl_resetDevice --> The MCU stops. Seems that it is hold in reset state. Until a power cycle applies. Not randomly, but 100%.
If I use serial_flash_programmer utility in stead of CCS & JTAG in Step 1, ie. flashing the MCU via UART, I won't see the issue in Step 3.
Do you have any idea of what is the root cause?
Regards,
Kien Nguyen