This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSCNCD28335: How to remove reset

Part Number: TMDSCNCD28335
Other Parts Discussed in Thread: UNIFLASH, TMS320F28335

Hi Team,

We need your help regarding the customer's concern below. I'm posting it on behalf of the customer. 

I was running some tests with the control card connected using docking station USB Emu R3. The control card was connected to my PC and my PC started to have low power (entered low power mode). I connected my PC charger and there was a spark on the outlet (it happens couple time with my charger) but after this the control card is stuck in reset mode and ask me to take it out with this error:

Error in build step #3 (Make): Make process exited with code 2:
"C:/ti/uniflash_7.2.0/dslite.bat" --flash --config=.\output_TI2833x\uniflash.ccxml .\output_TI2833x\Buck_Controller.out -u
Executing the following command:
> "C:\ti\uniflash_7.2.0\deskdb\content\TICloudAgent\win\ccs_base\DebugServer\bin\DSLite" flash --flash --config=.\output_TI2833x\uniflash.ccxml .\output_TI2833x\Buck_Controller.out -u

For more details and examples, please refer to the UniFlash Quick Start guide.

error: C28xx: Failed CPU Reset: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: GEL: Error while executing OnReset(-1): Target failed to read register ST1
at (ST1&~(0x0100)) [f28335.gel:322]
at C28x_Mode() [f28335.gel:38]
at OnReset(-(1))
error: C28xx: GEL: Error while executing OnTargetConnect(): Reset failed: retcode=-1
at GEL_Reset() [f28335.gel:96]
at OnTargetConnect()
error: C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
info: C28xx: Flash Programmer: Warning: The configured device (TMS320F28335), does not match the detected device (). Flash Programming operations could be affected. Please consider modifying your target configuration file.
error: C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Failed CPU Reset: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Trouble Reading Register PC: (Error -1137 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Trouble Reading Register ST1: (Error -1137 @ 0x6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: GEL: Error while executing OnReset(-1): Target failed to read register ST1
at (ST1&~(0x0100)) [f28335.gel:322]
at C28x_Mode() [f28335.gel:38]
at OnReset(-(1))
error: C28xx: GEL: Error calling OnPreFileLoaded(): Reset failed: retcode=-1
error: C28xx: Trouble Writing Memory Block at 0xae0 on Page 1 of Length 0x1: (Error -1137 @ 0xAE1) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE0@Data
error: C28xx: Trouble Writing Memory Block at 0xae1 on Page 1 of Length 0x1: (Error -1137 @ 0xAE2) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE1@Data
error: C28xx: Trouble Writing Memory Block at 0xae2 on Page 1 of Length 0x1: (Error -1137 @ 0xAE3) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE2@Data
error: C28xx: Trouble Writing Memory Block at 0xae3 on Page 1 of Length 0x1: (Error -1137 @ 0xAE4) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE3@Data
error: C28xx: Trouble Writing Memory Block at 0xae4 on Page 1 of Length 0x1: (Error -1137 @ 0xAE5) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE4@Data
error: C28xx: Trouble Writing Memory Block at 0xae5 on Page 1 of Length 0x1: (Error -1137 @ 0xAE6) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE5@Data
error: C28xx: Trouble Writing Memory Block at 0xae6 on Page 1 of Length 0x1: (Error -1137 @ 0xAE7) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE6@Data
error: C28xx: Trouble Writing Memory Block at 0xae7 on Page 1 of Length 0x1: (Error -1137 @ 0xAE8) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 9.7.0.00213)
error: C28xx: Error occurred during flash operation: Target failed to write 0x00000AE7@Data
error: C28xx: Flash Programmer: Device is locked or not connected. Operation cancelled.
error: C28xx: File Loader: Memory write failed: Unknown error
Buck_Controller.mk:147: recipe for target 'download' failed

Failed: File: .\output_TI2833x\Buck_Controller.out: Load failed.
make: *** [download] Error 1

Best regards,

Jonathan

  • If the brownout happened during flash programming, it is possible the passwords are corrupted, in which case the only option is to replace the device on the Controlcard (or the Controlcard itself). It is also possible the device got damaged. 

    “stuck in reset mode” is not in itself a problem. If you poser-up a new device whose flash is empty, the WD will keep timing out and reset the device over and over again. If this is what is happening, one way to connect to the device would be to hold it in reset while connecting. If there is no reset switch, the SCI boot mode can be used.