This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: Question about CanaRegs.CAN_INT.bit.INT0ID

Part Number: TMS320F280039C


When testing CAN communication, the customer uses the timed interrupt function to poll "CanaRegs.CAN_INT.bit.INT0ID" to update data. When the customer uses mailbox 1-19, the CAN reception and transmission are normal.

However, when the customer uses mailbox 20 or more, it cannot trigger "CanaRegs.CAN_INT.bit.INT0ID", and it cannot enter the CAN processing program to update the received or sent data.

Can the "CanaRegs.CAN_INT.bit.INT0ID" bit not be triggered when using mailbox 20 or above? Is there any other way to solve it?

CAN initialization code:

void CanInit(void)
{
CAN_initModule(CAN_BASE);

CAN_enableInterrupt(CAN_BASE, CAN_INT_IE0 | CAN_INT_ERROR);


sCANAMailboxConfig();

CAN_startModule(CAN_BASE);

}