Part Number: TMS320F28379D
Other Parts Discussed in Thread: C2000WARE
Hi C2000 champs,
Could you indicate a TI document that describes the “proper” way of configuring a CSS project for C2000 target ?
For example, when configurating a C2K project/RAM based and following the “F2837xD Firmware Development Package User’s Guide” (F2837xD_FRM_EX_UG.pdf) located in the C2000Ware folder it seems that the additional steps (tweaks) for the FLASH build are missing.
There are also some conflicts between this user guide and the way that TI examples are configured :
- Output format : legacy COFF (user guide) eabi (examples)
- Support library : rts2800_fpu32.lib (user guide) libc.a (examples)
- Linker command file in General/project : empty (user guide) explicitly specified (examples)
- …
Any document which provides "official" guidances or help here would be very welcome !
Thank you!
Best,
Guillaume