Part Number: TMS320F28375S
Other Parts Discussed in Thread: LAUNCHXL-F28379D
Hello,
I have seen in the TMS320F28375S microcontroller's datasheet that Vddosc and Vdd must be powered on and off at the same time. There is also an advisory to check this in the datasheet.
As Vddosc is 3.3-V on-chip crystal oscillator X1 & X2 and the two zero-pin internal oscillators INTOSC and Vdd is 1,2V digital logic power pins, I guess that Vddio (3V3 digital I/O power pins) and Vdd (1,2V digital logic power pins) should be started at the same time.
On the other hand, after checking the EVAL BOARD LAUNCHXL-F28379D schematics, I see that 3V3 (VDDOSC, VDDA, VDDIO) is the source for 1V2 (VDD) voltage rail (3V3 Dc Dc Step-Down to 1V2).
So, I'm wondering whether I'm understanding well this datasheet recommendation or not.
Should 3V3 and 1V2 rails start at the same time or not? Should I follow the EVAL BOARD schematic or not?
Regards,