Part Number: TMS320F280049C-Q1
Hello,
I am referring Universal MotorControl Lab code I have following query. I am using PMSM motor with Hall effect sensor.
1. What should be the output voltage sensing format - L- Ll or L- N .My I need voltage sensing for all three phases and any specific hw filter required.
2.Is it ok If I am using Current transformer for Output current voltage sensing.
3. I am using Hall effect sensor . what is the need of MOTOR_SEEK_POS , MOTOR_ALIGNMENT .
4. what is the logic are used for the same because Hall effect sensor is always give us rotor angle.
5.what is the used of Motor Identification.
What is the difference between instaspin and FAST estimator . Which is better and easy to integrate.
Regards,