Other Parts Discussed in Thread: SYSCONFIG
Hi Champs,
I am asking for my customer.
The two comparators of CMPSS1 are used to judge the two protection conditions, and this two signals pass through OUTPUTXBAR to achieve the operation of logical OR, is the following achievable?
//myOUTPUTXBAR0 initialization
XBAR_setOutputLatchMode(XBAR_OUTPUT1, false);
XBAR_invertOutputSignal(XBAR_OUTPUT1, false);
//Mux-configuration
XBAR_setOutputMuxConfig(XBAR_OUTPUT1, XBAR_OUT_MUX00_CMPSS1_CTRIPOUTH); //A2/B6/PGA1_OF
XBAR_setOutputMuxConfig(XBAR_OUTPUT1, XBAR_OUT_MUX01_CMPSS1_CTRIPOUTL); //A3
XBAR_enableOutputMux(XBAR_OUTPUT1,XBAR_MUX00);
XBAR_enableOutputMux(XBAR_OUTPUT1,XBAR_MUX01);
GPIO_setDirectionMode(24, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(24, GPIO_PIN_TYPE_STD);
// GPIO_setQualificationMode(24, GPIO_QUAL_ASYNC);// No Qualified
GPIO_setPinConfig(GPIO_24_OUTPUTXBAR1);
Because I see this sentence as below:
The X-BAR allows the selection of a single signal or a logical OR of up to 32 signals