Part Number: TMS320F280025-Q1
Hi team!
flash of the F280025 can be partially or completely blocked with a 128-bit password, so that, for example, no readout via the debugger is possible.
Question:
1) Is some kind of anti-tamper logic programmed in, so that after 10 or x unlock attempts, for example, the flash is permanently blocked or deleted?
Or is it simply assumed that 2^128 unlock attempts are unlikely to crack a password?
2) Does a register exists, where unlock attempts are counted ?
BR