Part Number: LAUNCHXL-F280025C
Other Parts Discussed in Thread: C2000WARE, BOOSTXL-DRV8323RS, DAC128S085EVM
Hello,
We are running the LAUNCHXL-F280025C + BOOSTXL-DRV8323RS with a BLDC along with C2000Ware 4.01.00.00 & MotorControl SDK 4.00.00.00
While running Level 1 in the "universal_motorcontrol_lab_f28002x" project we are getting a voltage offset fault. Not sure how this is happening as Level 1 doesn't even have the motor connected and everything is "stock" with no modifications straight out of the box other than the steps required in the document to setup the two boards together.
See below data with offsets and faults. The ADC Voltage values are in the 20's. From what I understand they should be near zero and I assume this is what is throwing the fault? What's interesting is that when I manually clear the error and force the system to run the ADC voltage values go to ~ zero.
Any thoughts?