Part Number: TMS320F28377S
Hi,
I am using a target based on a tms320F28377S which is designed "Get / Flash" boot mode. When I load a code to the device, I get an error in this boot mode (screenshot given). But when boot mode is changed to "SCI" boot mode, the code is loaded to the device. Why cannot I load the code to the device in "Get / Flash" boot mode?
Also if a device was used in a boot mode, can it be used in a different boot mode again?


C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: Error occurred during flash operation: Timed out waiting for
target to halt while executing wr_pll.alg
C28xx_CPU1: Error writing the PLL values (Flash algorithm timed out).
Operation cancelled.
C28xx_CPU1: Perform a debugger reset and execute the Boot-ROM code (click
on the RESUME button in CCS debug window) before erasing/loading the
Flash. If that does not help to perform a successful Flash erase/load,
check the Reset cause (RESC) register, NMI shadow flag (NMISHDFLG)
register and the Boot-ROM status register for further debug.
C28xx_CPU1: File Loader: Memory write failed: Unknown error
C28xx_CPU1: GEL: File:
D:\Ph.D\14-Programming\MCU1U57V1.6\Flash_Option\MCU1U57V1.6.out: Load
failed.