Part Number: SCI
I've written a serial program in VS2017 that uploads the SCI_Bootloader (so I can write a program to flash) and when I load the SCI_Bootloader to the F28035 with the JTAG, everything works as expected. It reenters the SCI_Bootloader as seen by a quick blink of an LED prior to entering the main(), goes thru some setup and then it sits and waits for the flash file to be uploaded. (I removed the autobaud function and reprogrammed it to operate at 9600 baud. This works as I see all my bytes echoed back.) I can then use the VS2017 tool to upload the flash firmware thru the SCI port and operate as expected.
So when I remove the JTAG and Gnd GPIO37 and pull up GPIO34 to put the F28035 into SCI boot mode, I can apparently upload the SCI_Bootloader flash utility but when it is complete, I do not see the quick flash of the LEDs I expect to prior to the entry of main() and therefore my attempt to upload the flash file fails. It's as if the 'ENTRY POINT SYMBOL: "_c_int00" address: 000081c3' is not being entered
I pretty much follow the Figure 2-12. Overview of SCI_Boot Function in SPRUI10–December 2018 except for the autobaud. I have readjusted BRR for 9600 baud and it works fine.
I have tried to drop the map file into this ticket but it keeps disappearing. If any of that data is desired, I can copy it in.