Part Number: TMS320F280025C
Hi,
I have a bootloader, that works pretty decent when I don't use DCSM (Directly included in the project as here: https://www.ti.com/lit/an/spracp8a/spracp8a.pdf?ts=1656879106556)
My DCSM settings look like this:

The bootloader linker script is here:
-stack 0x380
MEMORY
{
BEGIN : origin = 0x080000, length = 0x000002
BOOT_RSVD : origin = 0x00000002, length = 0x00000126
RAMM0 : origin = 0x00000128, length = 0x000002D8
RAMM1 : origin = 0x00000400, length = 0x000003F8 /* on-chip RAM block M1 */
// RAMM1_RSVD : origin = 0x000007F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
/* RAMLS4 : origin = 0x0000A000, length = 0x00000800
RAMLS5 : origin = 0x0000A800, length = 0x00000800
RAMLS6 : origin = 0x0000B000, length = 0x00000800
RAMLS7 : origin = 0x0000B800, length = 0x00000800*/
/* Combining all the LS RAMs */
RAMLS4567 : origin = 0x0000A000, length = 0x00002000
RAMGS0 : origin = 0x0000C000, length = 0x000007F8
// RAMGS0_RSVD : origin = 0x0000C7F8, length = 0x00000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
BOOTROM : origin = 0x003F0000, length = 0x00008000
BOOTROM_EXT : origin = 0x003F8000, length = 0x00007FC0
RESET : origin = 0x003FFFC0, length = 0x00000002
/* Flash sectors */
/* BANK 0 */
FLASH_BANK0_SEC0 : origin = 0x080002, length = 0x000FFE /* on-chip Flash */
FLASH_BANK0_SEC1 : origin = 0x081000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC2 : origin = 0x082000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC3 : origin = 0x083000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC4 : origin = 0x084000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC5 : origin = 0x085000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC6 : origin = 0x086000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC7 : origin = 0x087000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC8 : origin = 0x088000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC9 : origin = 0x089000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC10 : origin = 0x08A000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC11 : origin = 0x08B000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC12 : origin = 0x08C000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC13 : origin = 0x08D000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC14 : origin = 0x08E000, length = 0x001000 /* on-chip Flash */
FLASH_BANK0_SEC15 : origin = 0x08F000, length = 0x000FF0 /* on-chip Flash */
// FLASH_BANK0_SEC15_RSVD : origin = 0x08FFF0, length = 0x000010 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */
}
SECTIONS
{
.reset : > RESET, TYPE = DSECT /* not used, */
codestart : > BEGIN, ALIGN(4)
.TI.ramfunc : LOAD = (FLASH_BANK0_SEC0 | FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2), /* This sector is loaded from flash to RAM */
RUN = RAMLS4567,
LOAD_START(RamfuncsLoadStart),
LOAD_SIZE(RamfuncsLoadSize),
LOAD_END(RamfuncsLoadEnd),
RUN_START(RamfuncsRunStart),
RUN_SIZE(RamfuncsRunSize),
RUN_END(RamfuncsRunEnd),
ALIGN(8)
.text : >> FLASH_BANK0_SEC0 | FLASH_BANK0_SEC1 | FLASH_BANK0_SEC2, ALIGN(8) /* Programm is in flash */
.cinit : > FLASH_BANK0_SEC2, ALIGN(4)
.switch : > FLASH_BANK0_SEC2, ALIGN(4)
.cio : > FLASH_BANK0_SEC2
.pinit : > FLASH_BANK0_SEC2 ALIGN(4)
.const : > FLASH_BANK0_SEC2, ALIGN(4)
.init_array : > FLASH_BANK0_SEC2, ALIGN(4)
.stack : > RAMM1
.bss : > RAMM0
.bss:output : > RAMM0
.bss:cio : > RAMM0
.data : > RAMM0 /* Seems not to work, when using AES data --> leads to CRC error while updating, why? --> Needs separate RAM */
.sysmem : > RAMM0
ramgs0 : > RAMGS0
/* Allocate IQ math areas: */
IQmath : > RAMM0
IQmathTables : > RAMM0
}
/*
//===========================================================================
// End of file.
//===========================================================================
*/
codestart.asm:
;//###########################################################################
;//
;// FILE: flash_kernel_ex3_codestartbranch.asm
;//
;// TITLE: Branch for redirecting code execution after boot.
;//
;// For these examples, code_start is the first code that is executed after
;// exiting the boot ROM code.
;//
;// The codestart section in the linker cmd file is used to physically place
;// this code at the correct memory location. This section should be placed
;// at the location the BOOT ROM will re-direct the code to. For example,
;// for boot to FLASH this code will be located at 0x80000.
;//
;// In addition, the example f28002x projects are setup such that the codegen
;// entry point is also set to the codestart label. This is done by linker
;// option -e in the project build options. When the debugger loads the code,
;// it will automatically set the PC to the "entry point" address indicated by
;// the -e linker option. In this case the debugger is simply assigning the PC,
;// it is not the same as a full reset of the device.
;//
;// The compiler may warn that the entry point for the project is other then
;// _c_init00. _c_init00 is the C environment setup and is run before
;// main() is entered. The codestart code will re-direct the execution
;// to _c_init00 and thus there is no worry and this warning can be ignored.
;//
;//###########################################################################
;// $Copyright:
;// Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
;//
;// Redistribution and use in source and binary forms, with or without
;// modification, are permitted provided that the following conditions
;// are met:
;//
;// Redistributions of source code must retain the above copyright
;// notice, this list of conditions and the following disclaimer.
;//
;// Redistributions in binary form must reproduce the above copyright
;// notice, this list of conditions and the following disclaimer in the
;// documentation and/or other materials provided with the
;// distribution.
;//
;// Neither the name of Texas Instruments Incorporated nor the names of
;// its contributors may be used to endorse or promote products derived
;// from this software without specific prior written permission.
;//
;// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
;// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
;// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
;// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
;// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
;// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
;// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
;// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
;// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
;// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
;// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
;// $
;//###########################################################################
***********************************************************************
WD_DISABLE .set 1 ;set to 1 to disable WD, else set to 0
.ref _c_int00
.ref main
.global load_app_jump_addr
.global code_start
.global ExitBoot
***********************************************************************
* Function: codestart section
*
* Description: Branch to code starting point
***********************************************************************
.sect "codestart"
.retain
code_start:
.if WD_DISABLE == 1
LB wd_disable ;Branch to watchdog disable code
.else
LB _c_int00 ;Branch to start of boot._asm in RTS library
;LCR main
.endif
;end codestart section
***********************************************************************
* Function: wd_disable
*
* Description: Disables the watchdog timer
***********************************************************************
.if WD_DISABLE == 1
.text
load_app_jump_addr:
LB ExitBoot
wd_disable:
SETC OBJMODE ;Set OBJMODE for 28x object code
EALLOW ;Enable EALLOW protected register access
MOVZ DP, #7029h>>6 ;Set data page for WDCR register
MOV @7029h, #0068h ;Set WDDIS bit in WDCR to disable WD
EDIS ;Disable EALLOW protected register access
LB _c_int00 ;Branch to start of boot._asm in RTS library
;LCR main
; Cleanup and exit. At this point the EntryAddr
; is located in the ACC register
;BF ExitBoot, UNC
.endif
;end wd_disable
;loadApplication:
; Cleanup and exit. At this point the EntryAddr
; is located in the ACC register
;BF ExitBoot, UNC
;-----------------------------------------------
; ExitBoot
;-----------------------------------------------
;-----------------------------------------------
;This module cleans up after the boot loader
;
; 1) Make sure the stack is deallocated.
; SP = 0x400 after exiting the boot
; loader
; 2) Push 0 onto the stack so RPC will be
; 0 after using LRETR to jump to the
; entry point
; 2) Load RPC with the entry point
; 3) Clear all XARn registers
; 4) Clear ACC, P and XT registers
; 5) LRETR - this will also clear the RPC
; register since 0 was on the stack
;-----------------------------------------------
ExitBoot:
__stack: .usect ".stack",0
;-----------------------------------------------
; Insure that the stack is deallocated
;-----------------------------------------------
MOV SP,#__stack
;-----------------------------------------------
; Clear the bottom of the stack. This will endup
; in RPC when we are finished
;-----------------------------------------------
MOV *SP++,#0
MOV *SP++,#0
;-----------------------------------------------
; Load RPC with the entry point as determined
; by the boot mode. This address will be returned
; in the ACC register.
;-----------------------------------------------
PUSH ACC
POP RPC
;-----------------------------------------------
; Put registers back in their reset state.
;
; Clear all the XARn, ACC, XT, and P and DP
; registers
;
; NOTE: Leave the device in C28x operating mode
; (OBJMODE = 1, AMODE = 0)
;-----------------------------------------------
ZAPA
MOVL XT,ACC
MOVZ AR0,AL
MOVZ AR1,AL
MOVZ AR2,AL
MOVZ AR3,AL
MOVZ AR4,AL
MOVZ AR5,AL
MOVZ AR6,AL
MOVZ AR7,AL
MOVW DP, #0
;------------------------------------------------
; Restore ST0 and ST1. Note OBJMODE is
; the only bit not restored to its reset state.
; OBJMODE is left set for C28x object operating
; mode.
;
; ST0 = 0x0000 ST1 = 0x0A0B
; 15:10 OVC = 0 15:13 ARP = 0
; 9: 7 PM = 0 12 XF = 0
; 6 V = 0 11 M0M1MAP = 1
; 5 N = 0 10 reserved
; 4 Z = 0 9 OBJMODE = 1
; 3 C = 0 8 AMODE = 0
; 2 TC = 0 7 IDLESTAT = 0
; 1 OVM = 0 6 EALLOW = 0
; 0 SXM = 0 5 LOOP = 0
; 4 SPA = 0
; 3 VMAP = 1
; 2 PAGE0 = 0
; 1 DBGM = 1
; 0 INTM = 1
;-----------------------------------------------
MOV *SP++,#0
MOV *SP++,#0x0A0B
POP ST1
POP ST0
;------------------------------------------------
; Jump to the EntryAddr as defined by the
; boot mode selected and continue execution
;-----------------------------------------------
LRETR
;eof ----------
.end
;//
;// End of file.
;//
So, how it comes, that the reset does not work anymore? Does DCSM somehow shift all the address and it cannot jump to start?