Other Parts Discussed in Thread: LAUNCHXL-F280039C
Hello Ti experts,
I built a PCB featuring C2000's F280039C chip. The schematic mostly follows the LAUNCHXL-F280039C design except for the clocking, where I decided to only use the internal oscillator.

I left X1(GPIO19) and X2(GPIO18) floating on the PCB. Is this a mistake?
After loading a small test program, I get stuck at this line in ccs:

Here are some more details about my application:
-I am using XDS110 Debug probe
-Both 3.3V and 1.2V rails seem to work fine.
-The JTAG integrity test is successful
-The nRESET signal interrupts the debug session correctly when pulled low
-The emu (all 4) signals on the probe are left floating
Finally, is this mistake fixable by clever soldering?