Part Number: CCSTUDIO-C2000
Other Parts Discussed in Thread: C2000WARE
Hi Team,
Is there any command line statements to check which CCS and C2000Ware versions are installed in Linux?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: CCSTUDIO-C2000
Other Parts Discussed in Thread: C2000WARE
Hi Team,
Is there any command line statements to check which CCS and C2000Ware versions are installed in Linux?
Hi,
The version numbers are mentioend in the folder names where CCS and C2000Ware are installed.
For e.g: C2000Ware v4.01.00.00 will be installed by default into C2000Ware_4_01_00_00. Similarly CCS v12.0 is installed into ccs1200.
Best Regards
Siddharth
Hi Siddharth,
I want to know if there is a command line function to know if these tools are installed. The above details will be helpful if I know that CCS and C2000ware are installed in a particular location.
Kind regards,
Irene
Irene,
There are no such command line functions available.
Best Regards
Siddharth