Other Parts Discussed in Thread: TMS320F28055
Hello folks,
I have a question about the ADC on the TMS320F28055 controller. I connected a 100 kiloohm potentiometer (3.3V) to the ADC. For testing purposes I took the example from TI. I wanted to trigger my ADC on a timer interrupt, so I set the BIT AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 1, 1 is the timer 0 if I run the program as in the example, I can also see in debug mode that the ADCRESULT0 value changes. Does anyone know why the value changes even though I haven't initialized Timer0? Another question would be how can my ADC interrupt be triggered? I saw in debug mode that the interrupt is not called at all, but the ADCRESULT0 value changes. When I turn my potentiometer all the way up I only see a value of 3796 does that mean the ADC was calibrated incorrectly? Sorry for the many questions, but this is the first time I've used an ADC with the TI controller.
thank you for your help
// Included Files
//
#include "DSP28x_Project.h" // Device Headerfile and Examples Include File
//
// Function Prototypes
//
__interrupt void adc_isr(void);
//
// Global variables
//
Uint16 LoopCount;
Uint16 ConversionCount;
Uint16 Voltage1[10] = {0,0,0,0,0,0,0,0,0,0};
Uint16 Voltage2[10];
main()
{
//
// Step 1. Initialize System Control:
// PLL, WatchDog, enable Peripheral Clocks
// This example function is found in the F2805x_SysCtrl.c file.
//
InitSysCtrl();
//
// Step 2. Initialize GPIO:
// This example function is found in the F2805x_Gpio.c file and
// illustrates how to set the GPIO to it's default state.
//
// InitGpio(); // Skipped for this example
//
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable CPU interrupts
//
DINT;
//
// Initialize the PIE control registers to their default state.
// The default state is all PIE interrupts disabled and flags
// are cleared.
// This function is found in the F2805x_PieCtrl.c file.
//
InitPieCtrl();
//
// Disable CPU interrupts and clear all CPU interrupt flags
//
IER = 0x0000;
IFR = 0x0000;
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
// This will populate the entire table, even if the __interrupt
// is not used in this example. This is useful for debug purposes.
// The shell ISR routines are found in F2805x_DefaultIsr.c.
// This function is found in F2805x_PieVect.c.
//
InitPieVectTable();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
EALLOW; // This is needed to write to EALLOW protected register
PieVectTable.ADCINT1 = &adc_isr;
EDIS; // This is needed to disable write to EALLOW protected registers
//
// Step 4. Initialize all the Device Peripherals:
//
InitAdc(); // For this example, init the ADC
AdcOffsetSelfCal();
//
// Step 5. User specific code, enable __interrupts:
//
// Enable ADCINT1 in PIE
//
PieCtrlRegs.PIEIER1.bit.INTx1 = 1; // Enable INT 1.1 in the PIE
IER |= M_INT1; // Enable CPU Interrupt 1
EINT; // Enable Global __interrupt INTM
ERTM; // Enable Global realtime __interrupt DBGM
LoopCount = 0;
ConversionCount = 0;
//
// Configure ADC
// Notes:
// Channel ADCINA4 will be double sampled to workaround the ADC 1st
// sample issue for rev0 silicon errata.
// Due to round-robin, SOC0 converts first, then SOC1, then SOC2
//
EALLOW;
AdcRegs.ADCCTL1.bit.INTPULSEPOS= 1; //ADCINT1 trips after AdcResults latch
AdcRegs.INTSEL1N2.bit.INT1E = 1; //Enabled ADCINT1
AdcRegs.INTSEL1N2.bit.INT1CONT = 0; //Disable ADCINT1 Continuous mode
AdcRegs.INTSEL1N2.bit.INT1SEL = 2; //setup EOC2 to trigger ADCINT1
AdcRegs.ADCSOC0CTL.bit.CHSEL = 4; //set SOC0 channel select to ADCINA4
// AdcRegs.ADCSOC1CTL.bit.CHSEL = 4; //set SOC1 channel select to ADCINA4
// AdcRegs.ADCSOC2CTL.bit.CHSEL = 2; //set SOC2 channel select to ADCINA2
AdcRegs.ADCSOC0CTL.bit.TRIGSEL = 1; //TIMER0 //set SOC0 start trigger on EPWM1A
// AdcRegs.ADCSOC1CTL.bit.TRIGSEL = 5; //set SOC1 start trigger on EPWM1A
// AdcRegs.ADCSOC2CTL.bit.TRIGSEL = 5; //set SOC2 start trigger on EPWM1A
AdcRegs.ADCSOC0CTL.bit.ACQPS = 9; //SOC0 S/H Window = 10 (9+1) Clk Cycles SAMPLE Size
// AdcRegs.ADCSOC1CTL.bit.ACQPS = 9; //SOC0 S/H Window = 10 (9+1) Clk Cycles
// AdcRegs.ADCSOC2CTL.bit.ACQPS = 9; //SOC0 S/H Window = 10 (9+1) Clk Cycles
EDIS;
//
// Wait for ADC __interrupt
//
for(;;)
{
LoopCount++;
}
}
__interrupt void adc_isr(void)
{
//
//Discard ADCRESULT0 as part of the workaround to rev0's 1st sample errata
//
Voltage1[ConversionCount] = AdcResult.ADCRESULT0;
// Voltage2[ConversionCount] = AdcResult.ADCRESULT2;
//
// If 10 conversions have been logged, start over
//
if(ConversionCount == 9)
{
ConversionCount = 0;
}
else
{
ConversionCount++;
}
//
// Clear ADCINT1 flag reinitialize for next SOC
//
AdcRegs.ADCINTFLGCLR.bit.ADCINT1 = 1;
PieCtrlRegs.PIEACK.all = PIEACK_GROUP1; // Acknowledge __interrupt to PIE
return;
}