This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: Migrating from TMS320F280041C to TMS320F280039C

Part Number: TMS320F280039C
Other Parts Discussed in Thread: TMS320F280041C, , TMDSHVMTRINSPIN, C2000WARE, TIDM-02010

Dear Ti,

We are Migrating from TMS320F280041C to TMS320F280039C and we had used tmdshvmtrinspin reference solution and now we want to use TMS320F280039C. We are using C2000Ware_MotorControl_SDK_3_00_01_00 for our existing project. We want reference solution for TMS320F280039C. Also we will require 

1. DCSM Linker file

2. Equivalant f28004x_flash_cpu_is.cmd file

3. Equivalant f28004x_dcsm_z1otp.asm file

 

Anup

  • I'd recommend downloading MC SDK 4.00.00. We've added a F28003x project for the TIDM-02010 reference design. Unlike the F28004x, we don't support InstaSPIN-FOC in ROM on the F28003x, so you'll need to use a .lib version of the InstaSPIN-FOC code, which is demonstrated in the TIDM-02010 code.

    We also have the Universal Motor Control Lab project which supports F28002x only at the moment, but it also uses the InstaSPIN-FOC .lib and supports the TMDSHVMTRINSPIN board, so it could be a good reference. We plan on releasing an F28003x version of the Universal Lab, but it won't be until later this year.

    Whitney