This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-1000: Vienna Rectifier - step down

Part Number: TIDM-1000

Hi Team,

We received this inquiry from our customer.

Would like to inquire about the TIDM-1000 eval brd.

One of the designed outputs for this eval brd is 600 V with a 3 phase 208 Vrms Line to Line or 120 Vrms Line to Neutral input. 

Have noticed much of the calibration and instruction is based on the 120 Vrms Line to neutral value. 

What would be the lowest output voltage that could be designed for with this topology? 

Would it be based off of the pk of the Line to Neutral or Line to Line voltage?

If it is desired to lower the VBus what is the best way to go about doing this if this is possible?

Does TI have a topology for a "Buck" version of the Vienna Rectifier?

Regards,

Danilo