Part Number: TMS320F28384D
//#############################################################################
//
// FILE: can_ex5_transmit_receive.c
//
// TITLE: CAN Configuration for Transmit and Receive.
//
//! \addtogroup driver_example_list
//! <h1> CAN Transmit and Receive Configurations </h1>
//!
//! This example shows the basic setup of CAN in order to transmit or receive
//! messages on the CAN bus with a specific Message ID. The CAN Controller is
//! configured according to the selection of the define.
//!
//! When the TRANSMIT define is selected, the CAN Controller acts as a
//! Transmitter and sends data to the second CAN Controller connected
//! externally.If TRANMSIT is not defined the CAN Controller acts as a Receiver
//! and waits for message to be transmitted by the External CAN Controller.
//! Please refer to the appnote Programming Examples and Debug Strategies
//! for the DCAN Module (www.ti.com/lit/SPRACE5) for useful information
//! about this example
//!
//! \note CAN modules on the device need to be connected to via CAN
//! transceivers.
//!
//! \b Hardware \b Required \n
//! - A C2000 board with CAN transceiver.
//!
//! \b External \b Connections \n
//! - ControlCARD CANA is on DEVICE_GPIO_PIN_CANTXA (CANTXA)
//! - and DEVICE_GPIO_PIN_CANRXA (CANRXA)
//!
//! \b Watch \b Variables \b Transmit \Configuration \n
//! - MSGCOUNT - Adjust to set the number of messages
//! - txMsgCount - A counter for the number of messages sent
//! - txMsgData - An array with the data being sent
//! - errorFlag - A flag that indicates an error has occurred
//! - rxMsgCount - Has the initial value as No. of Messages to be received
//! and decrements with each message.
//!
//
//#############################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
//
// Comment to Make the CAN Controller work as a Receiver.
//
//#define TRANSMIT
//
// Defines
//
#ifdef TRANSMIT
#define TX_MSG_OBJ_ID 1
#else
#define RX_MSG_OBJ_ID 1
#endif
#define MSG_DATA_LENGTH 8
#define MSGCOUNT 10000000000
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
#define IPC_CMD_READ_MEM 0x1001
#define IPC_CMD_RESP 0x2001
#define TEST_PASS 0x5555
#define TEST_FAIL 0xAAAA
#define PACKET_LENGTH 10
#pragma DATA_SECTION(packetData, "MSGRAM_CPU_TO_CM")
uint8_t packetData[PACKET_LENGTH];
uint32_t pass;
uint32_t readData[10];
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
//
// Globals
//
#ifdef TRANSMIT
volatile uint32_t txMsgCount = 0;
uint32_t txMsgSuccessful = 1;
uint16_t txMsgData[4];
#else
volatile uint32_t rxMsgCount = MSGCOUNT;
uint8_t els;
uint8_t fi;
uint16_t rxMsgData[8];
#endif
volatile unsigned long i;
volatile uint32_t errorFlag = 0;
//
// Function Prototypes
//
__interrupt void canaISR(void);
//
// Main
//
void main(void)
{
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
int i;
IPC_MessageQueue_t messageQueue;
IPC_Message_t TxMsg, RxMsg;
//
// Initialize device clock and peripherals
//
Device_init();
////////////////////
Device_bootCM(BOOTMODE_BOOT_TO_S0RAM);
/////////////////////
//
// Initialize GPIO and configure GPIO pins for CANTX/CANRX
// on module A.
//
Device_initGPIO();
/////////////////////////////////
SysCtl_setEnetClk(SYSCTL_ENETCLKOUT_DIV_2, SYSCTL_SOURCE_SYSPLL);
// SysCtl_setEnetClk(SYSCTL_ENETCLKOUT_DIV_2, SYSCTL_SOURCE_SYSPLL);
/////////////////////////////////
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANRXA);
GPIO_setPinConfig(DEVICE_GPIO_CFG_CANTXA);
/////////////////////////////////////////////
GPIO_setPinConfig(GPIO_42_ENET_MDIO_CLK);
GPIO_setPinConfig(GPIO_43_ENET_MDIO_DATA);
GPIO_setPinConfig(GPIO_40_ENET_MII_CRS);
GPIO_setPinConfig(GPIO_41_ENET_MII_COL);
GPIO_setPinConfig(GPIO_75_ENET_MII_TX_DATA0);
GPIO_setPinConfig(GPIO_60_ENET_MII_TX_DATA1);
GPIO_setPinConfig(GPIO_61_ENET_MII_TX_DATA2);
GPIO_setPinConfig(GPIO_62_ENET_MII_TX_DATA3);
GPIO_setPinConfig(GPIO_45_ENET_MII_TX_EN);
GPIO_setPinConfig(GPIO_63_ENET_MII_RX_DATA0);
GPIO_setPinConfig(GPIO_53_ENET_MII_RX_DATA1);
GPIO_setPinConfig(GPIO_54_ENET_MII_RX_DATA2);
GPIO_setPinConfig(GPIO_66_ENET_MII_RX_DATA3);
GPIO_setPinConfig(GPIO_65_ENET_MII_RX_ERR);
GPIO_setPinConfig(GPIO_64_ENET_MII_RX_DV);
GPIO_setPinConfig(GPIO_44_ENET_MII_TX_CLK);
GPIO_setPinConfig(GPIO_49_ENET_MII_RX_CLK);
GPIO_setDirectionMode(68, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(68, GPIO_PIN_TYPE_PULLUP);
GPIO_writePin(68,1);
GPIO_setDirectionMode(57, GPIO_DIR_MODE_OUT);
GPIO_setPadConfig(57, GPIO_PIN_TYPE_PULLUP);
GPIO_writePin(57,1);
/////////////////////////////////////////////
//
// Allocated shared peripheral to C28x
//
SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_CAN_A,0x0U);
// SysCtl_allocateSharedPeripheral(SYSCTL_PALLOCATE_CAN_B,0x0U);
//
// Initialize the CAN controllers
//
CAN_initModule(CANA_BASE);
//
// Set up the CAN bus bit rate to 500kHz for each module
// Refer to the Driver Library User Guide for information on how to set
// tighter timing control. Additionally, consult the device data sheet
// for more information about the CAN module clocking.
//
CAN_setBitRate(CANA_BASE, DEVICE_SYSCLK_FREQ, 500000, 16);
//
// Enable interrupts on the CAN A peripheral.
//
CAN_enableInterrupt(CANA_BASE, CAN_INT_IE0 | CAN_INT_ERROR |
CAN_INT_STATUS);
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// Enable Global Interrupt (INTM) and realtime interrupt (DBGM)
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
IPC_clearFlagLtoR(IPC_CPU1_L_CM_R, IPC_FLAG_ALL);
IPC_initMessageQueue(IPC_CPU1_L_CM_R, &messageQueue, IPC_INT1, IPC_INT1);
IPC_sync(IPC_CPU1_L_CM_R, IPC_FLAG31);
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
//
EINT;
ERTM;
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
for(i=0; i<10; i++)
{
readData[i] = i;
}
//
// Update the message
//
TxMsg.command = IPC_CMD_READ_MEM;
TxMsg.address = (uint32_t)readData;
TxMsg.dataw1 = 10; // Using dataw1 as data length
TxMsg.dataw2 = 1; // Message identifier
//
// Send message to the queue
// Since C28x and CM does not share the same address space for shared RAM,
// ADDRESS_CORRECTION is enabled
//
IPC_sendMessageToQueue(IPC_CPU1_L_CM_R, &messageQueue, IPC_ADDR_CORRECTION_ENABLE,
&TxMsg, IPC_BLOCKING_CALL);
//
// Read message from the queue
// Return message from CM does not use the address field, hence
// ADDRESS_COREECTION feature is not used
//
IPC_readMessageFromQueue(IPC_CPU1_L_CM_R, &messageQueue, IPC_ADDR_CORRECTION_DISABLE,
&RxMsg, IPC_BLOCKING_CALL);
if((RxMsg.command == IPC_CMD_RESP) && (RxMsg.dataw1 == TEST_PASS) && (RxMsg.dataw2 == 1))
pass = 1;
else
pass = 0;
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
// This registers the interrupt handler in PIE vector table.
//
Interrupt_register(INT_CANA0,&canaISR);
//
// Enable the CAN-A interrupt signal
//
Interrupt_enable(INT_CANA0);
CAN_enableGlobalInterrupt(CANA_BASE, CAN_GLOBAL_INT_CANINT0);
#ifdef TRANSMIT
//
// Initialize the transmit message object used for sending CAN messages.
// Message Object Parameters:
// CAN Module: A
// Message Object ID Number: 1
// Message Identifier: 0x15555555
// Message Frame: Extended
// Message Type: Transmit
// Message ID Mask: 0x0
// Message Object Flags: None
// Message Data Length: 4 Bytes
//
CAN_setupMessageObject(CANA_BASE, TX_MSG_OBJ_ID, 0x15555555,
CAN_MSG_FRAME_EXT, CAN_MSG_OBJ_TYPE_TX, 0,
CAN_MSG_OBJ_TX_INT_ENABLE, MSG_DATA_LENGTH);
//
// Initialize the transmit message object data buffer to be sent
//
txMsgData[0] = 0x12;
txMsgData[1] = 0x34;
txMsgData[2] = 0x56;
txMsgData[3] = 0x78;
#else
//
// Initialize the receive message object used for receiving CAN messages.
// Message Object Parameters:
// CAN Module: A
// Message Object ID Number: 1
// Message Identifier: 0x15555555
// Message Frame: Extended
// Message Type: Receive
// Message ID Mask: 0x0
// Message Object Flags: Receive Interrupt
// Message Data Length: 4 Bytes (Note that DLC field is a "don't care"
// for a Receive mailbox
//
CAN_setupMessageObject(CANA_BASE, RX_MSG_OBJ_ID, 0x15555555,
CAN_MSG_FRAME_EXT, CAN_MSG_OBJ_TYPE_RX, 0,
CAN_MSG_OBJ_RX_INT_ENABLE, MSG_DATA_LENGTH);
#endif
//
// Start CAN module A operations
//
CAN_startModule(CANA_BASE);
#ifdef TRANSMIT
//
// Transmit messages from CAN-A.
//
for(i = 0; i < MSGCOUNT; i++)
{
//
// Check the error flag to see if errors occurred
//
if(errorFlag)
{
asm(" ESTOP0");
}
//
// Transmit the message.
//
CAN_sendMessage(CANA_BASE, TX_MSG_OBJ_ID, MSG_DATA_LENGTH,
txMsgData);
//
// Delay 0.25 second before continuing
//
DEVICE_DELAY_US(250000);
while(txMsgSuccessful);
//
// Increment the value in the transmitted message data.
//
txMsgData[0] += 0x01;
txMsgData[1] += 0x01;
txMsgData[2] += 0x01;
txMsgData[3] += 0x01;
//
// Reset data if exceeds a byte
//
if(txMsgData[0] > 0xFF)
{
txMsgData[0] = 0;
}
if(txMsgData[1] > 0xFF)
{
txMsgData[1] = 0;
}
if(txMsgData[2] > 0xFF)
{
txMsgData[2] = 0;
}
if(txMsgData[3] > 0xFF)
{
txMsgData[3] = 0;
}
//
// Update the flag for next message.
//
txMsgSuccessful = 1;
}
#else
//
// Loop to keep receiving data from another CAN Controller.
//
while(rxMsgCount)
{
}
#endif
//
// Stop application after completion.
//
asm(" ESTOP0");
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
while(1);
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
}
//
// CAN A ISR - The interrupt service routine called when a CAN interrupt is
// triggered on CAN module A.
//
__interrupt void
canaISR(void)
{
uint32_t status;
//
// Read the CAN-B interrupt status to find the cause of the interrupt
//
status = CAN_getInterruptCause(CANA_BASE);
//
// If the cause is a controller status interrupt, then get the status
//
if(status == CAN_INT_INT0ID_STATUS)
{
//
// Read the controller status. This will return a field of status
// error bits that can indicate various errors. Error processing
// is not done in this example for simplicity. Refer to the
// API documentation for details about the error status bits.
// The act of reading this status will clear the interrupt.
//
status = CAN_getStatus(CANA_BASE);
//
// Check to see if an error occurred.
//
#ifdef TRANSMIT
if(((status & ~(CAN_STATUS_TXOK)) != CAN_STATUS_LEC_MSK) &&
((status & ~(CAN_STATUS_TXOK)) != CAN_STATUS_LEC_NONE))
#else
if(((status & ~(CAN_STATUS_RXOK)) != CAN_STATUS_LEC_MSK) &&
((status & ~(CAN_STATUS_RXOK)) != CAN_STATUS_LEC_NONE))
#endif
{
//
// Set a flag to indicate some errors may have occurred.
//
errorFlag = 1;
}
}
#ifdef TRANSMIT
else if(status == TX_MSG_OBJ_ID)
{
//
// Getting to this point means that the TX interrupt occurred on
// message object 1, and the message TX is complete. Clear the
// message object interrupt.
//
CAN_clearInterruptStatus(CANA_BASE, TX_MSG_OBJ_ID);
//
// Increment a counter to keep track of how many messages have been
// transmitted. In a real application this could be used to set flags to
// indicate when a message is transmitted.
//
txMsgCount++;
//
// Since the message was transmitted, clear any error flags.
//
errorFlag = 0;
//
// Clear the message transmitted successful Flag.
//
txMsgSuccessful = 0;
}
#else
else if(status == RX_MSG_OBJ_ID)
{
//
// Get the received message
//
CAN_readMessage(CANA_BASE, RX_MSG_OBJ_ID, rxMsgData);
//
// Getting to this point means that the RX interrupt occurred on
// message object 1, and the message RX is complete. Clear the
// message object interrupt.
//
CAN_clearInterruptStatus(CANA_BASE, RX_MSG_OBJ_ID);
//
// Decrement the counter after a message has been received.
//
rxMsgCount--;
//
// Since the message was received, clear any error flags.
//
errorFlag = 0;
}
#endif
//
// If something unexpected caused the interrupt, this would handle it.
//
else
{
//
// Spurious interrupt handling can go here.
//
}
//
// Clear the global interrupt flag for the CAN interrupt line
//
CAN_clearGlobalInterruptStatus(CANA_BASE, CAN_GLOBAL_INT_CANINT0);
//
// Acknowledge this interrupt located in group 9
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP9);
}
//
// End of File
//
Here I have attached codes that i am used.I have combined codes for CAN, remote processor communication and Ethernet.I would like to receive data from CAN and send it through Ethernet please help on this. (I am new to TI controller programming) If I am wrong means please suggest a example for my exact application.Thanks in advance!
//###########################################################################
//
// FILE: enet_lwip.c
//
// TITLE: lwIP based Ethernet Example.
//
// Example to demonstrate UDP socket (for daikin customer)
// buf_rx,buf_tx are the watch variables which can be used or updated in the
// main application based on the requirement.
//
// Test setup
//
// F2838x Control Card connected to a PC/laptop on the Ethernet port.
// PC/laptop runs the SocketTest/’Packet Sender’ software, configured for the IP Address and port . \
// Keywords ‘START’ and ‘STOP’ are used to send and stop receiving messages respectively
// Received data is stored in ‘buf_rx’ array and data to be transmitted is stored in ‘buf_tx’ array on CM core of F2838x device
// Examples is Interrupt based with a callback function ‘udp_rx_callback’ which handles the received data from the SocketTest/Packet Sender software.
//
//###########################################################################
// $TI Release: $
// $Release Date: $
// $Copyright:
// Copyright (C) 2022 Texas Instruments Incorporated - http://www.ti.com
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
#include <string.h>
#include "inc/hw_ints.h"
#include "inc/hw_memmap.h"
#include "inc/hw_nvic.h"
#include "inc/hw_types.h"
#include "inc/hw_sysctl.h"
#include "inc/hw_emac.h"
#include "driverlib_cm/ethernet.h"
#include "driverlib_cm/gpio.h"
#include "driverlib_cm/interrupt.h"
#include "driverlib_cm/flash.h"
#include "driverlib_cm/sysctl.h"
#include "driverlib_cm/systick.h"
#include "utils/lwiplib.h"
#include "board_drivers/pinout.h"
#include "lwipopts.h"
#include "ipc.h"
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
#include "ipc.h"
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
#define PAYLOAD 35
volatile uint32_t msTime=0;
volatile bool flag_TX_frame_UDP=true;
#define MAKE_IP_ADDRESS(a0,a1,a2,a3) (((a0<<24) & 0xFF000000) | ((a1<<16) & 0x00FF0000) | ((a2<<8) & 0x0000FF00) | (a3 & 0x000000FF) )
bool Connected_udp_28000 = false;
uint16_t cnt_Connected_udp_28000 = 0;
uint8_t ISR;
uint8_t VAl;
//uint16_t buf_rx;
// Defines
//
#define PACKET_LENGTH 132
struct udp_pcb *g_upcb;
u8_t buf_rx[PAYLOAD];
u8_t buf_tx[PAYLOAD];
char * buf_tx_start_msg = "Something to show UDP is working \n";
uint32_t buf_tx_start_msg_count = 35;
uint16_t cont_rx_udp = 0;
struct pbuf *pbuf1_tx;
//*****************************************************************************
//
//! \addtogroup master_example_list
//! <h1>Ethernet with lwIP (enet_lwip)</h1>
//!
//! This example application demonstrates the operation of the F2838x
//! microcontroller Ethernet controller using the lwIP TCP/IP Stack. Once
//! programmed, the device sits endlessly waiting for ICMP ping requests. It
//! has a static IP address. To ping the device, the sender has to be in the
//! same network. The stack also supports ARP.
//!
//! For additional details on lwIP, refer to the lwIP web page at:
//! http://savannah.nongnu.org/projects/lwip/
//
//*****************************************************************************
// These are defined by the linker (see device linker command file)
extern uint16_t RamfuncsLoadStart;
extern uint16_t RamfuncsLoadSize;
extern uint16_t RamfuncsRunStart;
extern uint16_t RamfuncsLoadEnd;
extern uint16_t RamfuncsRunEnd;
extern uint16_t RamfuncsRunSize;
extern uint16_t constLoadStart;
extern uint16_t constLoadEnd;
extern uint16_t constLoadSize;
extern uint16_t constRunStart;
extern uint16_t constRunEnd;
extern uint16_t constRunSize;
#define DEVICE_FLASH_WAITSTATES 2
//*****************************************************************************
//
// Driver specific initialization code and macro.
//
//*****************************************************************************
#define ETHERNET_NO_OF_RX_PACKETS 2U
#define ETHERNET_MAX_PACKET_LENGTH 1538U
#define NUM_PACKET_DESC_RX_APPLICATION PBUF_POOL_SIZE //8 - same as PBUF_POOL_SIZE
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
#define IPC_CMD_READ_MEM 0x1001
#define IPC_CMD_RESP 0x2001
#define TEST_PASS 0x5555
#define TEST_FAIL 0xAAAA
bool status = false;
uint32_t command,add,data;
uint8_t ipisr;
uint8_t ipif;
uint8_t ips;
uint8_t ipi;
IPC_MessageQueue_t messageQueue;
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
Ethernet_Handle emac_handle;
Ethernet_InitConfig *pInitCfg;
uint32_t Ethernet_numRxCallbackCustom = 0;
uint32_t releaseTxCount = 0;
uint32_t genericISRCustomcount = 0;
uint32_t genericISRCustomRBUcount = 0;
uint32_t genericISRCustomROVcount = 0;
uint32_t genericISRCustomRIcount = 0;
uint32_t systickPeriodValue = 125000; //15000000;
Ethernet_Pkt_Desc pktDescriptorRXCustom[NUM_PACKET_DESC_RX_APPLICATION];
extern uint32_t Ethernet_numGetPacketBufferCallback;
extern Ethernet_Device Ethernet_device_struct;
uint8_t Ethernet_rxBuffer[ETHERNET_NO_OF_RX_PACKETS *
ETHERNET_MAX_PACKET_LENGTH];
uint32_t sendPacketFailedCount = 0;
uint8_t mac_custom[6] = {0xA8, 0x63, 0xF2, 0x00, 0x1D, 0x98};
extern Ethernet_Pkt_Desc*
lwIPEthernetIntHandler(Ethernet_Pkt_Desc *pPacket);
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
__interrupt void IPC_ISR1()
{
int i;
IPC_Message_t TxMsg, RxMsg;
bool status = false;
//
// Read the message from the message queue
//
IPC_readMessageFromQueue(IPC_CM_L_CPU1_R, &messageQueue, IPC_ADDR_CORRECTION_ENABLE,
&RxMsg, IPC_NONBLOCKING_CALL);
if(RxMsg.command == IPC_CMD_READ_MEM)
{
status = true;
//
// Read and compare data
//
for(i=0; i<RxMsg.dataw1; i++)
{
if((*(uint32_t *)RxMsg.address + i) != i)
status = false;
}
}
//
// Send response message
//
TxMsg.command = IPC_CMD_RESP;
TxMsg.address = 0; // Not used
TxMsg.dataw1 = status ? TEST_PASS : TEST_FAIL;
TxMsg.dataw2 = RxMsg.dataw2; // Use the message identifier from the received message
IPC_sendMessageToQueue(IPC_CM_L_CPU1_R, &messageQueue, IPC_ADDR_CORRECTION_DISABLE,
&TxMsg, IPC_NONBLOCKING_CALL);
//
// Acknowledge the flag
//
IPC_ackFlagRtoL(IPC_CM_L_CPU1_R, IPC_FLAG1);
}
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
void CM_init(void)
{
//
// Disable the watchdog
//
SysCtl_disableWatchdog();
#ifdef _FLASH
//
// Copy time critical code and flash setup code to RAM. This includes the
// following functions: InitFlash();
//
// The RamfuncsLoadStart, RamfuncsLoadSize, and RamfuncsRunStart symbols
// are created by the linker. Refer to the device .cmd file.
// Html pages are also being copied from flash to ram.
//
memcpy(&RamfuncsRunStart, &RamfuncsLoadStart, (size_t)&RamfuncsLoadSize);
memcpy(&constRunStart, &constLoadStart, (size_t)&constLoadSize);
//
// Call Flash Initialization to setup flash waitstates. This function must
// reside in RAM.
//
Flash_initModule(FLASH0CTRL_BASE, FLASH0ECC_BASE, DEVICE_FLASH_WAITSTATES);
#endif
//
// Sets the NVIC vector table offset address.
//
#ifdef _FLASH
Interrupt_setVectorTableOffset((uint32_t)vectorTableFlash);
#else
Interrupt_setVectorTableOffset((uint32_t)vectorTableRAM);
#endif
}
//*****************************************************************************
//
// HTTP Webserver related callbacks and definitions.
//
//*****************************************************************************
//
// Currently, this implemented as a pointer to function which is called when
// corresponding query is received by the HTTP webserver daemon. When more
// features are needed to be added, it should be implemented as a separate
// interface.
//
void httpLEDToggle(void);
void(*ledtoggleFuncPtr)(void) = &httpLEDToggle;
//*****************************************************************************
//
// The interrupt handler for the SysTick interrupt.
//
//*****************************************************************************
void
SysTickIntHandler(void)
{
//
// Call the lwIP timer handler.
//
// lwIPTimer(systickPeriodValue);
lwIPTimer(1);
}
//*****************************************************************************
//
// This function is a callback function called by the example to
// get a Packet Buffer. Has to return a ETHERNET_Pkt_Desc Structure.
// Rewrite this API for custom use case.
//
//*****************************************************************************
Ethernet_Pkt_Desc* Ethernet_getPacketBufferCustom(void)
{
//
// Get the next packet descriptor from the descriptor pool
//
uint32_t shortIndex = (Ethernet_numGetPacketBufferCallback + 3)
% NUM_PACKET_DESC_RX_APPLICATION;
//
// Increment the book-keeping pointer which acts as a head pointer
// to the circular array of packet descriptor pool.
//
Ethernet_numGetPacketBufferCallback++;
//
// Update buffer length information to the newly procured packet
// descriptor.
//
pktDescriptorRXCustom[shortIndex].bufferLength =
ETHERNET_MAX_PACKET_LENGTH;
//
// Update the receive buffer address in the packer descriptor.
//
pktDescriptorRXCustom[shortIndex].dataBuffer =
&Ethernet_device_struct.rxBuffer [ \
(ETHERNET_MAX_PACKET_LENGTH*Ethernet_device_struct.rxBuffIndex)];
//
// Update the receive buffer pool index.
//
Ethernet_device_struct.rxBuffIndex += 1U;
Ethernet_device_struct.rxBuffIndex = \
(Ethernet_device_struct.rxBuffIndex%ETHERNET_NO_OF_RX_PACKETS);
//
// Receive buffer is usable from Address 0
//
pktDescriptorRXCustom[shortIndex].dataOffset = 0U;
//
// Return this new descriptor to the driver.
//
return (&(pktDescriptorRXCustom[shortIndex]));
}
//*****************************************************************************
//
// This is a hook function and called by the driver when it receives a
// packet. Application is expected to replenish the buffer after consuming it.
// Has to return a ETHERNET_Pkt_Desc Structure.
// Rewrite this API for custom use case.
//
//*****************************************************************************
Ethernet_Pkt_Desc* Ethernet_receivePacketCallbackCustom(
Ethernet_Handle handleApplication,
Ethernet_Pkt_Desc *pPacket)
{
Ethernet_Pkt_Desc* temp_eth_pkt;
//
// Book-keeping to maintain number of callbacks received.
//
#ifdef ETHERNET_DEBUG
Ethernet_numRxCallbackCustom++;
#endif
Ethernet_disableRxDMAReception(EMAC_BASE,0);
//
// This is a placeholder for Application specific handling
// We are replenishing the buffer received with another buffer
//
// return lwIPEthernetIntHandler(pPacket);
temp_eth_pkt=lwIPEthernetIntHandler(pPacket);
Ethernet_enableRxDMAReception(EMAC_BASE,0);
return temp_eth_pkt;
}
void Ethernet_releaseTxPacketBufferCustom(
Ethernet_Handle handleApplication,
Ethernet_Pkt_Desc *pPacket)
{
//
// Once the packet is sent, reuse the packet memory to avoid
// memory leaks. Call this interrupt handler function which will take care
// of freeing the memory used by the packet descriptor.
//
lwIPEthernetIntHandler(pPacket);
//
// Increment the book-keeping counter.
//
#ifdef ETHERNET_DEBUG
releaseTxCount++;
#endif
}
Ethernet_Pkt_Desc *Ethernet_performPopOnPacketQueueCustom(
Ethernet_PKT_Queue_T *pktQueuePtr)
{
Ethernet_Pkt_Desc *pktDescHdrPtr;
pktDescHdrPtr = pktQueuePtr->head;
if(0U != pktDescHdrPtr)
{
pktQueuePtr->head = pktDescHdrPtr->nextPacketDesc;
pktQueuePtr->count--;
}
return(pktDescHdrPtr);
}
void Ethernet_performPushOnPacketQueueCustom(
Ethernet_PKT_Queue_T *pktQueuePtr,
Ethernet_Pkt_Desc *pktDescHdrPtr)
{
pktDescHdrPtr->nextPacketDesc = 0U;
if(0U == pktQueuePtr->head)
{
//
// Queue is empty - Initialize it with this one packet
//
pktQueuePtr->head = pktDescHdrPtr;
pktQueuePtr->tail = pktDescHdrPtr;
}
else
{
//
// Queue is not empty - Push onto END
//
pktQueuePtr->tail->nextPacketDesc = pktDescHdrPtr;
pktQueuePtr->tail = pktDescHdrPtr;
}
pktQueuePtr->count++;
}
void Ethernet_setMACConfigurationCustom(uint32_t base, uint32_t flags)
{
HWREG(base + ETHERNET_O_MAC_CONFIGURATION) |= flags;
}
void Ethernet_clearMACConfigurationCustom(uint32_t base, uint32_t flags)
{
HWREG(base + ETHERNET_O_MAC_CONFIGURATION) &= ~flags;
}
interrupt void Ethernet_genericISRCustom(void)
{
ISR++;
genericISRCustomcount++;
Ethernet_RxChDesc *rxChan;
Ethernet_TxChDesc *txChan;
Ethernet_HW_descriptor *descPtr;
Ethernet_HW_descriptor *tailPtr;
uint16_t i=0;
Ethernet_clearMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
Ethernet_clearMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_TE);
for(i = 0U;i < Ethernet_device_struct.initConfig.numChannels;i++)
{
Ethernet_disableRxDMAReception(
Ethernet_device_struct.baseAddresses.enet_base,
i);
}
if(((ETHERNET_DMA_CH0_STATUS_AIS |
ETHERNET_DMA_CH0_STATUS_RBU) ==
(HWREG(Ethernet_device_struct.baseAddresses.enet_base +
ETHERNET_O_DMA_CH0_STATUS) &
(uint32_t)(ETHERNET_DMA_CH0_STATUS_AIS |
ETHERNET_DMA_CH0_STATUS_RBU))) ||
(ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS) ==
(HWREG(Ethernet_device_struct.baseAddresses.enet_base +
ETHERNET_O_MTL_Q0_INTERRUPT_CONTROL_STATUS) &
(uint32_t)(ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS
)))
{
if((ETHERNET_DMA_CH0_STATUS_AIS |
ETHERNET_DMA_CH0_STATUS_RBU) ==
(HWREG(Ethernet_device_struct.baseAddresses.enet_base +
ETHERNET_O_DMA_CH0_STATUS) &
(uint32_t)(ETHERNET_DMA_CH0_STATUS_AIS |
ETHERNET_DMA_CH0_STATUS_RBU)))
{
genericISRCustomRBUcount++;
}
if((ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS) ==
(HWREG(Ethernet_device_struct.baseAddresses.enet_base +
ETHERNET_O_MTL_Q0_INTERRUPT_CONTROL_STATUS) &
(uint32_t)(ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS
)))
{
genericISRCustomROVcount++;
Ethernet_enableMTLInterrupt(Ethernet_device_struct.baseAddresses.enet_base,0,
ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOVFIS);
}
/*
* Clear the AIS and RBU status bit. These MUST be
* cleared together!
*/
Ethernet_clearDMAChannelInterrupt(
Ethernet_device_struct.baseAddresses.enet_base,
ETHERNET_DMA_CHANNEL_NUM_0,
ETHERNET_DMA_CH0_STATUS_AIS |
ETHERNET_DMA_CH0_STATUS_RBU);
/*
*Recover from Receive Buffer Unavailable (and hung DMA)
*
* All descriptor buffers are owned by the application, and
* in result the DMA cannot transfer incoming frames to the
* buffers (RBU condition). DMA has also entered suspend
* mode at this point, too.
*
* Drain the RX queues
*/
/* Upon RBU error, discard all previously received packets */
if(Ethernet_device_struct.initConfig.pfcbDeletePackets != NULL)
(*Ethernet_device_struct.initConfig.pfcbDeletePackets)();
rxChan =
&Ethernet_device_struct.dmaObj.rxDma[ETHERNET_DMA_CHANNEL_NUM_0];
txChan=
&Ethernet_device_struct.dmaObj.txDma[ETHERNET_DMA_CHANNEL_NUM_0];
/*
* Need to disable multiple interrupts, so protect the code to do so within
* a global disable block (to prevent getting interrupted in between)
*/
if(NULL!= Ethernet_device_struct.ptrPlatformInterruptDisable)
{
(*Ethernet_device_struct.ptrPlatformInterruptDisable)(
Ethernet_device_struct.interruptNum[
ETHERNET_RX_INTR_CH0 + rxChan->chInfo->chNum]);
(*Ethernet_device_struct.ptrPlatformInterruptDisable)(
Ethernet_device_struct.interruptNum[
ETHERNET_GENERIC_INTERRUPT]);
}
/* verify we have full capacity in the descriptor queue */
if(rxChan->descQueue.count < rxChan->descMax) {
/* The queue is not at full capacity due to OOM errors.
Try to fill it again */
Ethernet_addPacketsIntoRxQueue(rxChan);
}
Ethernet_initRxChannel(
&Ethernet_device_struct.initConfig.chInfo[ETHERNET_CH_DIR_RX][0]);
Ethernet_writeRxDescTailPointer(
Ethernet_device_struct.baseAddresses.enet_base,
0,
(&Ethernet_device_struct.rxDesc[
((uint32_t)ETHERNET_DESCRIPTORS_NUM_RX_PER_CHANNEL) *
(0 + (uint32_t)1U)]));
if(NULL!= Ethernet_device_struct.ptrPlatformInterruptEnable)
{
(*Ethernet_device_struct.ptrPlatformInterruptEnable)(
Ethernet_device_struct.interruptNum[
ETHERNET_RX_INTR_CH0 + rxChan->chInfo->chNum]);
(*Ethernet_device_struct.ptrPlatformInterruptEnable)(
Ethernet_device_struct.interruptNum[
ETHERNET_GENERIC_INTERRUPT]);
}
}
if(0U != (HWREG(Ethernet_device_struct.baseAddresses.enet_base +
ETHERNET_O_DMA_CH0_STATUS) &
(uint32_t) ETHERNET_DMA_CH0_STATUS_RI))
{
genericISRCustomRIcount++;
Ethernet_clearDMAChannelInterrupt(
Ethernet_device_struct.baseAddresses.enet_base,
ETHERNET_DMA_CHANNEL_NUM_0,
ETHERNET_DMA_CH0_STATUS_NIS | ETHERNET_DMA_CH0_STATUS_RI);
}
for(i = 0U;i < Ethernet_device_struct.initConfig.numChannels;i++)
{
Ethernet_enableRxDMAReception(
Ethernet_device_struct.baseAddresses.enet_base,
i);
}
Ethernet_setMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
Ethernet_setMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_TE);
}
void
Ethernet_init(const unsigned char *mac)
{
Ethernet_InitInterfaceConfig initInterfaceConfig;
uint32_t macLower;
uint32_t macHigher;
uint8_t *temp;
initInterfaceConfig.ssbase = EMAC_SS_BASE;
initInterfaceConfig.enet_base = EMAC_BASE;
initInterfaceConfig.phyMode = ETHERNET_SS_PHY_INTF_SEL_MII;
//
// Assign SoC specific functions for Enabling,Disabling interrupts
// and for enabling the Peripheral at system level
//
initInterfaceConfig.ptrPlatformInterruptDisable =
&Platform_disableInterrupt;
initInterfaceConfig.ptrPlatformInterruptEnable =
&Platform_enableInterrupt;
initInterfaceConfig.ptrPlatformPeripheralEnable =
&Platform_enablePeripheral;
initInterfaceConfig.ptrPlatformPeripheralReset =
&Platform_resetPeripheral;
//
// Assign the peripheral number at the SoC
//
initInterfaceConfig.peripheralNum = SYSCTL_PERIPH_CLK_ENET;
//
// Assign the default SoC specific interrupt numbers of Ethernet interrupts
//
initInterfaceConfig.interruptNum[0] = INT_EMAC;
initInterfaceConfig.interruptNum[1] = INT_EMAC_TX0;
initInterfaceConfig.interruptNum[2] = INT_EMAC_TX1;
initInterfaceConfig.interruptNum[3] = INT_EMAC_RX0;
initInterfaceConfig.interruptNum[4] = INT_EMAC_RX1;
pInitCfg = Ethernet_initInterface(initInterfaceConfig);
Ethernet_getInitConfig(pInitCfg);
pInitCfg->dmaMode.InterruptMode = ETHERNET_DMA_MODE_INTM_MODE2;
//
// Assign the callbacks for Getting packet buffer when needed
// Releasing the TxPacketBuffer on Transmit interrupt callbacks
// Receive packet callback on Receive packet completion interrupt
//
pInitCfg->pfcbRxPacket = &Ethernet_receivePacketCallbackCustom;
pInitCfg->pfcbGetPacket = &Ethernet_getPacketBuffer; //custom
pInitCfg->pfcbFreePacket = &Ethernet_releaseTxPacketBufferCustom;
//
//Assign the Buffer to be used by the Low level driver for receiving
//Packets. This should be accessible by the Ethernet DMA
//
pInitCfg->rxBuffer = Ethernet_rxBuffer;
//
// The Application handle is not used by this application
// Hence using a dummy value of 1
//
Ethernet_getHandle((Ethernet_Handle)1, pInitCfg , &emac_handle);
//
// Disable transmit buffer unavailable and normal interrupt which
// are enabled by default in Ethernet_getHandle.
//
Ethernet_disableDmaInterrupt(Ethernet_device_struct.baseAddresses.enet_base,
0, (ETHERNET_DMA_CH0_INTERRUPT_ENABLE_TBUE |
ETHERNET_DMA_CH0_INTERRUPT_ENABLE_NIE));
//
// Enable the MTL interrupt to service the receive FIFO overflow
// condition in the Ethernet module.
//
Ethernet_enableMTLInterrupt(Ethernet_device_struct.baseAddresses.enet_base,0,
ETHERNET_MTL_Q0_INTERRUPT_CONTROL_STATUS_RXOIE);
//
// Disable the MAC Management counter interrupts as they are not used
// in this application.
//
HWREG(Ethernet_device_struct.baseAddresses.enet_base + ETHERNET_O_MMC_RX_INTERRUPT_MASK) = 0xFFFFFFFF;
HWREG(Ethernet_device_struct.baseAddresses.enet_base + ETHERNET_O_MMC_IPC_RX_INTERRUPT_MASK) = 0xFFFFFFFF;
//
//Do global Interrupt Enable
//
(void)Interrupt_enableInProcessor();
//
//Assign default ISRs
//
Interrupt_registerHandler(INT_EMAC_TX0, Ethernet_transmitISR);
Interrupt_registerHandler(INT_EMAC_RX0, Ethernet_receiveISR);
Interrupt_registerHandler(INT_EMAC, Ethernet_genericISRCustom);
//
// Convert the mac address string into the 32/16 split variables format
// that is required by the driver to program into hardware registers.
// Note: This step is done after the Ethernet_getHandle function because
// a dummy MAC address is programmed in that function.
//
temp = (uint8_t *)&macLower;
temp[0] = mac[0];
temp[1] = mac[1];
temp[2] = mac[2];
temp[3] = mac[3];
temp = (uint8_t *)&macHigher;
temp[0] = mac[4];
temp[1] = mac[5];
//
// Program the unicast mac address.
//
Ethernet_setMACAddr(EMAC_BASE,
0,
macHigher,
macLower,
ETHERNET_CHANNEL_0);
Ethernet_clearMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
Ethernet_setMACConfigurationCustom(Ethernet_device_struct.baseAddresses.enet_base,ETHERNET_MAC_CONFIGURATION_RE);
}
void udp_rx_callback(void *arg, struct udp_pcb *upcb, struct pbuf *p,
struct ip_addr *addr, u16_t port)
{
char *cad_rx;
uint16_t long_actual = 0;
uint16_t long_UDP_complete = 0;
uint16_t long_total = 0;
uint8_t cnt_lee = 0;
httpLEDToggle();
memset(buf_rx, 0x00, 50);
long_total = p->tot_len;
cont_rx_udp++;
while ((long_UDP_complete < long_total)
&& (long_UDP_complete < 1800) || (cnt_lee == 0))
{
cnt_lee++;
long_actual = p->len;
cad_rx = p->payload;
int i = 0;
for (i = 0; i < long_actual; i++)
{
buf_rx[0 + i + long_UDP_complete] = *cad_rx++;
}
long_UDP_complete = long_actual + long_UDP_complete;
buf_rx[long_UDP_complete + 1] = '\n';
if (long_UDP_complete == long_total)
{
pbuf_free(p); //* don't leak the pbuf!
}
else
{
if ( p->next != NULL)
p = p->next;
// pbuf_free(a); /* don't leak the pbuf!*/
}
if ((buf_rx[0] == 'S') && (buf_rx[1] == 'T') && (buf_rx[2] == 'O') && (buf_rx[3] == 'P'))
{ //Disconnect
//udp_disconnect(upcb);
Connected_udp_28000 = false;
cnt_Connected_udp_28000 = 0;
}
else if ((buf_rx[0] == 'S') && (buf_rx[1] == 'T') && (buf_rx[2] == 'A') && (buf_rx[3] == 'R') && (buf_rx[4] == 'T'))
{ //Connect
Connected_udp_28000 = true;
cnt_Connected_udp_28000 = 0;
/* process the payload in p->payload */
udp_connect(upcb, addr, port); /* connect to the remote host */
}
}
pbuf_free(p);
if (!Connected_udp_28000)
{
udp_disconnect(upcb);
}
}
/* UDP initialization ......................................................*/
void my_udp_init(void)
{
g_upcb = udp_new();
udp_bind(g_upcb, IP_ADDR_ANY, 28000);
udp_recv(g_upcb, &udp_rx_callback, (void*) 0);
}
//*****************************************************************************
//
// This example demonstrates the use of the Ethernet Controller.
//
//*****************************************************************************
//unsigned long IPAddr = 0xC0A80004; // 0xC0A80004; //192.168.0.4
unsigned long IPAddr = 0xC300004D;
unsigned long NetMask = 0xFFFFFF00;
unsigned long GWAddr = 0x00000000;
int
main(void)
{
unsigned long ulUser0, ulUser1;
unsigned char pucMACArray[8];
int i=0;
// ////////////////////////////////////////
// Initializing the CM. Loading the required functions to SRAM.
//
CM_init();
SYSTICK_setPeriod(systickPeriodValue);
SYSTICK_enableCounter();
SYSTICK_registerInterruptHandler(SysTickIntHandler);
SYSTICK_enableInterrupt();
//
// Enable processor interrupts.
//
Interrupt_enableInProcessor();
// Set user/company specific MAC octets
// (for this code we are using A8-63-F2-00-00-80)
// 0x00 MACOCT3 MACOCT2 MACOCT1
ulUser0 = 0x00F263A8;
// 0x00 MACOCT6 MACOCT5 MACOCT4
ulUser1 = 0x00800000;
//
// Convert the 24/24 split MAC address from NV ram into a 32/16 split MAC
// address needed to program the hardware registers, then program the MAC
// address into the Ethernet Controller registers.
//
pucMACArray[0] = ((ulUser0 >> 0) & 0xff);
pucMACArray[1] = ((ulUser0 >> 8) & 0xff);
pucMACArray[2] = ((ulUser0 >> 16) & 0xff);
pucMACArray[3] = ((ulUser1 >> 0) & 0xff);
pucMACArray[4] = ((ulUser1 >> 8) & 0xff);
pucMACArray[5] = ((ulUser1 >> 16) & 0xff);
//
// Initialize ethernet module.
//
Ethernet_init(pucMACArray);
//
// Initialze the lwIP library, using DHCP.
//
lwIPInit(0, pucMACArray, IPAddr, NetMask, GWAddr, IPADDR_USE_STATIC);
// Initialize the UDP server
//
my_udp_init();
//
// Loop forever. All the work is done in interrupt handlers.
//
uint32_t cnt_FFT = 0;
Interrupt_setPriority(INT_EMAC_TX0, 2);
Interrupt_setPriority(INT_EMAC_RX0, 1);
Interrupt_enable(INT_EMAC_TX0);
Interrupt_enable(INT_EMAC_RX0);
Interrupt_enable(INT_EMAC);
volatile int cnt_total_loop=0;
volatile int cnt_total_mqtt_pub=0;
while (1)
{
cnt_total_loop++;
if (Connected_udp_28000)
{
//UDP TX block
if (flag_TX_frame_UDP)
{
cnt_FFT++;
flag_TX_frame_UDP = false;
/*
/////////////////////////////////////////////
for (i = 0; i < PAYLOAD; i++)
{
if(i < buf_tx_start_msg_count)
{
buf_tx[i] = (uint8_t)buf_tx_start_msg[i];
}
else
{
buf_tx[i] = (uint8_t) (cnt_FFT);
}
}
*/
////////////////////////////////////////////
pbuf1_tx = pbuf_alloc(PBUF_TRANSPORT, PAYLOAD, PBUF_RAM);
if (pbuf1_tx!= NULL)
{
pbuf1_tx->payload = (void*) buf_tx ;
pbuf1_tx->tot_len = PAYLOAD; //17 // long_UDP_complete+4;
pbuf1_tx->len = PAYLOAD; //17 // long_UDP_complete+4;
udp_send(g_upcb, pbuf1_tx);
}
cnt_Connected_udp_28000++;
if (pbuf1_tx!= NULL)
pbuf_free(pbuf1_tx);
}
}
SysCtl_delay(6000000);//aprox 1 sec
sys_check_timeouts();
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
IPC_clearFlagLtoR(IPC_CM_L_CPU1_R, IPC_FLAG_ALL);
//
// Enable IPC interrupts
//
IPC_registerInterrupt(IPC_CM_L_CPU1_R, IPC_INT0, IPC_ISR0);
//
// Synchronize both the cores.
//
IPC_sync(IPC_CM_L_CPU1_R, IPC_FLAG31);
//
// Loop forever. Wait for IPC interrupt
//
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
}
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
// while(1);
//!!!!!!!!!!!!!!!!!!!!!!!!!!!!!
}
//*****************************************************************************
//
// Called by lwIP Library. Toggles the led when a command is received by the
// HTTP webserver.
//
//*****************************************************************************
void httpLEDToggle(void)
{
//
// Toggle the LED D1 on the control card.
//
GPIO_togglePin(DEVICE_GPIO_PIN_LED1);
}
//*****************************************************************************
//
// Called by lwIP Library. Could be used for periodic custom tasks.
//
//*****************************************************************************
uint32_t cnt_ms_lwip_Htimer=0;
uint32_t cnt_ms_TX_Htimer=0;
void lwIPHostTimerHandler(void)
{
// msTime++;
cnt_ms_lwip_Htimer++;
}