Part Number: TIDM-1000
Other Parts Discussed in Thread: POWERSUITE
Hello,
I have a question on the Design Guide TIDM-1000 of Vienna Rectifier-Based, Three-Phase Power Factor Correction (PFC) Reference Design Using C2000 MCU.
Specifically it is on Section 6.4.3.1 Setting Software Options for BUILD 3.
It is written in the Design Guide as follows:
" 4. Make sure the load connected at the output of the board is correctly entered on the powerSUITE syscfg page because this load value is used in the design of the voltage compensator."
However, on the powerSUITE syscfg page, I cannot find out any entry for the load connected at the output of the board.
Please review this issue for me.
Thank you for your advice.
With regards,
JS Yoo