Part Number: TIDM-1001
Hi
I am interested to modify this design with the following specifications -
- Input : 65V +/-1 V ( the modified TIDM 1001 will regulate the input voltage for this application )
- Output : 400V ( an external load will regulate the output voltage at 400V )
- Power :500W
I want this DC-DC converter to regulate the input voltage to 65V +/1 V , an external load module will regulate the output voltage to about 400V
Can you summarise the changes that will be required especially to the resonant components , the transformer and the software ?
How much work will be required make these changes ?
Regards
BJE