Part Number: TMS320F280049C
Other Parts Discussed in Thread: TMDSCNCD280049C, C2000WARE
Dear Sirs
I'm trying to get the interrupt_ex1_sw_prioritization example to compile and download into the TMDSCNCD280049C control card. The example project is located in C:\TI\c2000\C2000Ware_4_00_00_00\device_support\f28004x\examples\interrupts_ex1_sw_prioritization. Therefore, I would assume that everything is good to go. When I tried to compile the project, I get the following error message.
error #10234-D: unresolved symbols remain
error #10010: errors encountered during linking; "interrupts_ex1_sw_prioritization.out" not built
>> Compilation failure
makefile:150: recipe for target 'interrupts_ex1_sw_prioritization.out' failed
gmake[1]: *** [interrupts_ex1_sw_prioritization.out] Error 1
makefile:146: recipe for target 'all' failed
gmake: *** [all] Error 2
**** Build Finished ****
The default linker command file that the project uses is 280049M_RAM_lnk.cmd. knowing that the RAM space is much smaller than the FLASH space, I used 280049M_FLASH_lnk.cmd. The same error was reported. The control card uses the F280049C part. So I used the 280049C_FLASH_lnk.cmd. The same error was reported. I went to the C2000 forum and found a post that was 10 years old that had the same issue, program will not fit into available memory - C2000 microcontrollers forum - C2000︎ microcontrollers - TI E2E support forums. Trey German suggested using F28M35x_generic_M3_FLASH.cmd. This command file isn't in the dropdown listing but I did find F28M36x_generic_C28_FLASH.cmd and F28M36x_generic_wshared_C28_FLASH.cmd. Both of these command files work insofar as the project does compile. However, when I tried to download into the control card, I get the following error message,
C28xx_CPU1: GEL Output:
Memory Map Initialization Complete
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Start ...
C28xx_CPU1: GEL Output: ... DCSM Initialization Done ...
C28xx_CPU1: Loader: One or more sections of your program falls into a memory region that is not writable. These regions will not actually be written to the target. Check your linker configuration and/or memory map.
Any help is certainly appreciated. Thank you.