Part Number: TMS320F280025
Other Parts Discussed in Thread: C2000WARE-DIGITALPOWER-SDK
Hi Champs,
Here are customer's urgently issue as below:
Could you give me some suggestion/Dir?
#1.Customer are porting the code from F2802x to F28002x, they encounter the below figure showed compiler error.

And the console as print the follow info:
"C:\Users\ADMINI~1\AppData\Local\Temp\{E189B8AE-2B98-4C27-864B-23E4A7442F08}", ERROR!
at line 12810: [E0800] Instructions not permitted in structure/union definitions
ERROR .bits 1 ; bit field, 1 bits, 0 bit offset
#2, All Union-related definitions are not used in the R_Isr function, why is there an error related to illegal definition?