Part Number: TMS320F28069M
Other Parts Discussed in Thread: DRV8323
The DRV8323 has an enable signal that is connected to the TMS320. When the TMS320 goes through a software update, reset, or power-up/down condition the enable signal GPIO on the TMS320 is reconfigured as an input. This reconfiguration allows the DRV8323 to enable. We have the option of adding a strong pull-down on the enable signal to prevent the DRV8323 from enabling. The concern we have is to make sure that the three phase bridge is not being activated. Documentation for the TMS320 states that the PWM outputs are disabled during software update, reset, or power-up/down condition. Regardless of weather the DRV8323 is being enabled during a software update, reset, or power-up/down condition, the three phase bridge will not activate because the PWM outputs are disabled. Please verify our conclusion.